This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.STM32CubeMonitor allows to monitor several probes simultaneously, even if target are not similar.
In the example below, a Nucleo board L031K6 and a Discovery board F429ZI are used. Variables monitored are displayed in the same chart in the dashboard.
1. Design of the flow
Flows for each board are designed following method described in STM32CubeMonitor:How to configure mandatory parameters before acquisition.
Then Start and Stop buttons are connected to variable node for each board, and finally processing node for each board are connected to the chart node.
2. Dashboard view
The corresponding dashboard shows that both variables are monitored on the same chart, with a legend corresponding to the board, float1(myVariableL031) and float1(myVariableF429)