This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Highlight:
Displayed 50 items.
- STM32MP15 Discovery kits - starting for the first time (transclusion) (← links)
- STM32MP157x-DKx - software distributions (transclusion) (← links)
- STM32MP15 Discovery kits - required material (transclusion) (← links)
- STM32MP15 Discovery kits - Starter Package (transclusion) (← links)
- USBH device tree configuration (transclusion) (← links)
- I2C device tree configuration (transclusion) (← links)
- OTG device tree configuration (transclusion) (← links)
- How to display on HDMI (transclusion) (← links)
- How to create your own machine (transclusion) (← links)
- Bluetooth device tree configuration (transclusion) (← links)
- How to create your own image (transclusion) (← links)
- How to create your own distribution (transclusion) (← links)
- DAC device tree configuration (transclusion) (← links)
- DAC Linux driver (transclusion) (← links)
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- RNG device tree configuration (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- WLAN device tree configuration (transclusion) (← links)
- SPDIFRX device tree configuration (transclusion) (← links)
- DFSDM device tree configuration (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- Ethernet device tree configuration (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- USBPHYC device tree configuration (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- FDCAN device tree configuration (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to perform ssh connection (transclusion) (← links)
- Configfs (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- OpenSTLinux filesystem (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to play audio (transclusion) (← links)
- OpenSTLinux licenses (transclusion) (← links)
- Deep dive (transclusion) (← links)
- Reading tips (transclusion) (← links)
- How to assign an internal peripheral to an execution context (transclusion) (← links)
- Debugfs (transclusion) (← links)
- ALSA overview (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)
- How to cross-compile with the Distribution Package (transclusion) (← links)
- DRM KMS overview (transclusion) (← links)
- PHY overview (transclusion) (← links)