This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Highlight:
Displayed 50 items.
- How to update OTP with U-Boot (transclusion) (← links)
- How to configure U-Boot for your board (transclusion) (← links)
- Wiki archives (transclusion) (← links)
- TFLite Cpp image classification (transclusion) (← links)
- TFLite Cpp object detection (transclusion) (← links)
- X-LINUX-AI licenses (transclusion) (← links)
- TFLite Python image classification (transclusion) (← links)
- TFLite Python object detection (transclusion) (← links)
- Coral Cpp image classification (transclusion) (← links)
- Coral Python image classification (transclusion) (← links)
- Coral Cpp object detection (transclusion) (← links)
- Coral Python object detection (transclusion) (← links)
- How to run Coral Edge TPU inference using Python TensorFlow Lite API (transclusion) (← links)
- TAMP device tree configuration (transclusion) (← links)
- How to build and use an SDK for QT (transclusion) (← links)
- TFLite Cpp face recognition (transclusion) (← links)
- How to load U-Boot with STM32CubeProgrammer (transclusion) (← links)
- How to configure TF-A FW CONFIG (transclusion) (← links)
- STM32MP13 U-Boot (transclusion) (← links)
- STM32MP13 VREFBUF internal peripheral (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Populate the target and boot the image (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/What's next (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Install the SDK (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Modify, rebuild and reload the Linux® kernel (transclusion) (← links)
- How to load U-Boot with dfu-util (transclusion) (← links)
- STM32MP13 resources (transclusion) (← links)
- STM32MP13 V4L2 camera overview (transclusion) (← links)
- How to develop an X-Linux Expansion Package (transclusion) (← links)
- How to use UART as serial boot device with STM32CubeProgrammer (transclusion) (← links)
- Media-ctl (transclusion) (← links)
- STM32MP135x-DK - software distributions (transclusion) (← links)
- STM32MP13 Discovery kits - Starter Package (transclusion) (← links)
- STM32MP13 Discovery kits - required material (transclusion) (← links)
- STM32MP13 Discovery kits - starting for the first time (transclusion) (← links)
- How to measure performance of your NN models using the Coral Edge TPU (transclusion) (← links)
- How to measure performance of your NN models using TensorFlow Lite runtime (transclusion) (← links)
- How to add a new parallel or serial NAND flash memory device in Yocto (transclusion) (← links)
- X-NUCLEO-GNSS1A1 Expansion Board (transclusion) (← links)
- How to use U-Boot stm32key command (transclusion) (← links)
- How to perform Secure Boot from Distribution package (transclusion) (← links)
- STM32MP1 Developer Package - OpenSTLinux BSP (transclusion) (← links)
- How to secure STM32 MPU (transclusion) (← links)
- TF-A BL2 Trusted Board Boot (transclusion) (← links)
- STM32CubeMP15 Package release note - v1.6.0 (transclusion) (← links)
- How to build an example using libcoral API (transclusion) (← links)
- How to reproduce an example using PyCoral API (transclusion) (← links)
- STM32 MPU resources (transclusion) (← links)
- STM32PRGFW-UTIL (transclusion) (← links)
- How to deploy SSP: a step-by-step approach (transclusion) (← links)