This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Warning:
Displayed 50 items.
- STM32MP13 V4L2 camera overview (transclusion) (← links)
- How to develop an X-Linux Expansion Package (transclusion) (← links)
- IPCC device tree configuration (transclusion) (← links)
- STM32MP15 OTP mapping (transclusion) (← links)
- STM32MP13 Discovery kits - Starter Package (transclusion) (← links)
- STM32MP13 Discovery kits - required material (transclusion) (← links)
- STM32MP135x-DK - board assembly (transclusion) (← links)
- STM32MP135x-DK - board connections (transclusion) (← links)
- STM32MP13 Discovery kits - starting for the first time (transclusion) (← links)
- How to measure performance of your NN models using the Coral Edge TPU (transclusion) (← links)
- How to measure performance of your NN models using TensorFlow Lite runtime (transclusion) (← links)
- STM32MP13 OTP mapping (transclusion) (← links)
- How to install OPC UA (transclusion) (← links)
- STM32MP13 backup registers (transclusion) (← links)
- How to use U-Boot stm32key command (transclusion) (← links)
- Secure Firmware Update (transclusion) (← links)
- OP-TEE OTP overview (transclusion) (← links)
- PKA device tree configuration (transclusion) (← links)
- SAES device tree configuration (transclusion) (← links)
- How to perform Secure Boot from Distribution package (transclusion) (← links)
- STM32MP1 Developer Package - OpenSTLinux BSP (transclusion) (← links)
- How to secure STM32 MPU (transclusion) (← links)
- TF-A BL2 Trusted Board Boot (transclusion) (← links)
- Calibration device tree configuration (transclusion) (← links)
- STM32 MPU ecosystem release note - v4.0.0 (transclusion) (← links)
- STM32MP135x-DK - hardware description (transclusion) (← links)
- How to install and use the X-LINUX-AI SDK add-on (transclusion) (← links)
- How to build an example using libcoral API (transclusion) (← links)
- How to reproduce an example using PyCoral API (transclusion) (← links)
- How to create Signed FIT image from Distribution package (transclusion) (← links)
- STM32 MPU OpenSTLinux release note - v4.0.0 (transclusion) (← links)
- STM32DDRFW-UTIL (transclusion) (← links)
- STM32DDRFW-UTIL release note (transclusion) (← links)
- STM32PRGFW-UTIL (transclusion) (← links)
- STM32PRGFW-UTIL release note (transclusion) (← links)
- How to measure the performance of your models using ONNX Runtime (transclusion) (← links)
- Secure Secret Provisioning (SSP) (transclusion) (← links)
- How to deploy SSP: a step-by-step approach (transclusion) (← links)
- X-LINUX-AI - image classification using ONNX Python runtime (transclusion) (← links)
- STM32 MPU OpenSTLinux release note - v4.1.0 (transclusion) (← links)
- STM32 MPU ecosystem release note - v4.1.0 (transclusion) (← links)
- X-LINUX-AI OpenSTLinux Expansion Package - v2.2.0 (transclusion) (← links)
- X-LINUX-AI OpenSTLinux Expansion Package (transclusion) (← links)
- X-LINUX-AI - object detection using ONNX Python runtime (transclusion) (← links)
- X-LINUX-AI - object detection using ONNX C++ API (transclusion) (← links)
- Registered User (← links)
- Template:Green (transclusion) (← links)
- Template:Grey (transclusion) (← links)
- Template:Warning (transclusion) (← links)
- Template:SoftwareLicenseAgreement (transclusion) (← links)