This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article presents the recommended connections to start with the STM32MP135x-DK Discovery kit . Part numbers are specified in the STM32MP13 microprocessor part numbers article.


- MB1635 mother board :STM32MP135F 11x11, PMIC, DDR3
- MB1897 camera module
- Camera module flat cable
- microSD™ card slot
- Ethernet 2 → Network
- Ethernet 1 → Network
- USB Micro-B (STLINK-V3E) → PC Virtual COM port and debug
- USB Type-C™ (power 5V-3A)
- USB Type-C™ (DRP)
- 1st dual USB Type-A (host) → keyboard, mouse or USB driver
- 2nd dual USB Type-A (host) → keyboard, mouse or USB driver
- Reset button