This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This category groups together all articles that factorize information, and that are transcluded in other articles.
Sub-articles (in coordination with Template:InternalInfo) are also useful to isolate information that must not be visible outside STMicroelectronics.
Pages in category "Sub-articles"
The following 54 pages are in this category, out of 54 total.
D
P
S
- STM32 MPU boards
- STM32MP1 Developer Package - OpenSTLinux BSP
- STM32MP1 Developer Package - SDK
- STM32MP1 Developer Package - STM32CubeMP1 Package
- STM32MP1 Distribution Package - OpenSTLinux distribution
- STM32MP1 Starter Package - images
- STM32MP13 boards
- STM32MP13 Discovery kits - required material
- STM32MP13 Discovery kits - starting for the first time
- STM32MP13 internal peripherals assignment table template
- STM32MP13 internal peripherals software table template
- STM32MP135x-DK - board assembly
- STM32MP135x-DK - board connections
- STM32MP15 boards
- STM32MP15 Discovery kits - required material
- STM32MP15 Discovery kits - starting for the first time
- STM32MP15 Evaluation boards - required material
- STM32MP15 Evaluation boards - starting for the first time
- STM32MP15 internal peripherals assignment table template
- STM32MP15 internal peripherals software table template
- STM32MP157x-DKx - board assembly
- STM32MP157x-DKx - board connections
- STM32MP157x-EV1 - board assembly
- STM32MP157x-EV1 - board connections
- STM32MPU Embedded Software distribution
- Subpart - STM32MP1 - Starter Package