This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:=:
Displayed 50 items.
- How to display on HDMI (transclusion) (← links)
- How to create your own distribution (transclusion) (← links)
- DAC Linux driver (transclusion) (← links)
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- Hardware random overview (transclusion) (← links)
- GStreamer troubleshooting grid (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- How to customize the Linux kernel (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- Ethernet device tree configuration (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to integrate an external software package (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- How to perform ssh connection (transclusion) (← links)
- How to perform ping test (transclusion) (← links)
- Configfs (transclusion) (← links)
- How to configure a WLAN interface on hotspot mode (transclusion) (← links)
- WLAN and Bluetooth hardware component (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- How to set up a Bluetooth connection (transclusion) (← links)
- How to scan Bluetooth devices (transclusion) (← links)
- How to scan BLE devices (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- How to monitor the display framerate (transclusion) (← links)
- STM32MP15 resources (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to control a RNG in userspace (transclusion) (← links)
- How to retrieve Cortex-M4 logs after crash (transclusion) (← links)
- How to monitor the GCNANO GPU load (transclusion) (← links)
- DRM KMS troubleshooting grid (transclusion) (← links)
- How to play audio (transclusion) (← links)
- Reading tips (transclusion) (← links)
- How to assign an internal peripheral to an execution context (transclusion) (← links)
- Debugfs (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)
- How to cross-compile with the Distribution Package (transclusion) (← links)
- HDP Linux driver (transclusion) (← links)
- DRM KMS overview (transclusion) (← links)