Last edited 4 months ago

Buildroot-based Linux embedded software

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


Important
Buildroot-based Linux distribution is validated against the ecosystem release v6.2.0 (see release note). It will not be ported on ecosystem release v6.2.1 .
Partner program
Bootlin has developed specific support, demonstration configurations, and documentation to help ST customers use Buildroot on STM32 MPU platforms.

See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html

To address Bootlin technical support for Buildroot: mailto:buildroot-st-support@bootlin.com


The Buildroot-based Linux® embedded software is part of the STM32 MPU embedded software offer.
It is a set of software (see architecture overview), system build and development tools created to ease the development to be done on top of STM32 MPU devices.

It is made up of:

  • an open-source Linux® distribution, based on the Buildroot build system, running on the Arm® Cortex®-A processor(s),
  • firmwares, running on the Arm® Cortex®-M processor: FwST-M Packages (not available on STM32MP13x lines )

Buildroot[1] is a set of recipes and scripts that specify from where to download the source code of the different software components, and that allow to configure them, build them and finally install them.

The Linux® distribution relies on the OpenSTLinux board support package (U-Boot, TF-A, OP-TEE, Linux kernel) complemented with a user-space with a features set.

The partner's repository[2] is "Buildroot br2-external tree"[3] dedicated to supporting the STMicroelectronics STM32MPU platforms.

Several examples of Buildroot configurations [4] are provided:

  • the minimal configuration builds the TF-A firmware, U-Boot bootloader, Linux kernel and a minimal user-space composed of just Busybox,
  • more featureful configurations propose evolved demos

It also shows how device tree files generated by STM32CubeMX can be integrated in a Buildroot configuration, and proposes other guidelines for going further [5].



Buildroot release notesFwST-M PackagesLinux Buildroot-based embedded software

The Buildroot-based Linux embedded software offers three development packages that let developers select the support that best meets their needs:

  • the starter package to quickly and easily start with the boards. It delivers a software image (binary), ready to flash on an SD card, that includes pre-built examples (a.k.a. firmware) of the package(s) running on the Arm® Cortex®-M processor, running as coprocessor.
  • the developer package to add your own developments on top of the Buildroot-based Linux embedded software. It delivers:
    • the components of the board support package (BSP) in source code (e.g., Linux® kernel), and the software development kit (SDK), based on Buildroot SDK, for BSPs updates or cross-architecture applications development on an host PC,
    • the components of the software packages running on the Arm® Cortex®-M processor, running as coprocessor, in source code (e.g., STM32Cube MPU Package HAL), and the STM32CubeIDE as integrated development environment (IDE).
  • the distribution package to create your own Buildroot-based Linux® embedded software, as well as your own starter and developer packages. It delivers the source code of all the software components of the Buildroot-based Linux® embedded software, and uses the Buildroot as the underlying building and distribution generation framework.

STM32 supported device Boards Starter Package Developer Package Distribution Package Ecosystem release note
STM32MP13x lines  STM32MP13 Discovery kits STM32MPU Starter Package STM32MPU Developer Package Latest Buildroot tag: openstlinux-6.6-buildroot-2025.02.12-mpu-v26.02.18 Buildroot-based Linux ecosystem release note
STM32MP15x lines  STM32MP15 Discovery kits
STM32MP21x lines  STM32MP21 Discovery kits
STM32MP23x lines  STM32MP23 Discovery kits
STM32MP25x lines  STM32MP25 Evaluation boards
STM32MP25 Discovery kits

1. References[edit | edit source]