This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This category groups together all articles that are applicable for the STM32MP13x lines
Subcategories
This category has the following 7 subcategories, out of 7 total.
M
P
S
U
Pages in category "STM32MP13x"
The following 200 pages are in this category, out of 512 total.
(previous page) (next page)H
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage OpenSTLinux projects in STM32CubeIDE
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate and boot a board with OP-TEE
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to secure STM32 MPU
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to stop and start Weston
- How to stream camera over network
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to transfer a file over network
- How to transfer a file over serial console
- How to update OTP with U-Boot
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the Target Status widget in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
I
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- Interrupt overview
- IO expander hardware components
- IP Linux command line
- IWDG device tree configuration
- IWDG internal peripheral
L
- Latest wiki
- LEDs and buttons on STM32 MPU boards
- LegalInformation:Legal notice
- Linux application frameworks overview
- Linux tracing, monitoring and debugging
- LPTIM device tree configuration
- LPTIM internal peripheral
- LPTIM Linux driver
- LTDC device tree configuration
- LTDC internal peripheral
- Ltrace
- LTTng
M
N
O
- Online Linux trainings
- OP-TEE Calibration PTA overview
- OP-TEE OTP overview
- OP-TEE overview
- OPC UA overview
- OpenEmbedded
- OpenEmbedded - devtool
- OpenSTLinux architecture overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux directory structure
- OpenSTLinux distribution
- OpenSTLinux filesystem
- OpenSTLinux licenses
- LegalInformation:OpenSTLinux licenses - v4.0.0
- LegalInformation:OpenSTLinux licenses - v4.1.0
- OTG device tree configuration
- OTG internal peripheral
- Overview of GPIO pins
P
R
S
- SAES device tree configuration
- SAES internal peripheral
- SAI device tree configuration
- SAI internal peripheral
- SAI Linux driver
- SCMI device tree configuration
- SCMI overview
- SDK for OpenSTLinux distribution
- SDMMC device tree configuration
- SDMMC internal peripheral
- Secure Firmware Update
- Secure Secret Provisioning (SSP)
- Security overview
- Serial TTY device tree configuration
- Serial TTY overview
- Signing tool
- Signing tool release note
- SPDIFRX device tree configuration
- SPDIFRX internal peripheral
- SPDIFRX Linux driver
- SPI device tree configuration
- SPI internal peripheral
- SPI overview
- ST-LINK
- Standard SDK directory structure
- STGEN internal peripheral
- STM32 header for binary files
- STM32 MPU device tree
- STM32 MPU ecosystem release note
- STM32 MPU ecosystem release note - v4.0.0
- STM32 MPU ecosystem release note - v4.1.0
- STM32 MPU Flash mapping
- STM32 MPU Linux kernel overview
- STM32 MPU OpenSTLinux release note
- STM32 MPU OpenSTLinux release note - v4.0.0
- STM32 MPU OpenSTLinux release note - v4.0.0/Changes notification – v4.0.0
- STM32 MPU OpenSTLinux release note - v4.1.0
- STM32 MPU OpenSTLinux release note - v4.1.0/Changes notification – v4.1.0
- STM32 MPU OpenSTLinux release note/Changes notification
- STM32 MPU resources
- STM32 MPU ROM code overview
- STM32 MPU ROM code secure boot
- STM32 MPU ROM trace analyzer
- STM32 MPU trainings
- STM32 MPUs Community FAQ
- STM32CubeIDE
- STM32CubeIDE release note
- STM32CubeMX
- STM32CubeProgrammer
- STM32CubeProgrammer flashlayout
- STM32CubeProgrammer OTP management
- STM32CubeProgrammer release note
- STM32DDRFW-UTIL
- STM32DDRFW-UTIL release note
- STM32MP1 Developer Package
- STM32MP1 Developer Package - SDK
- STM32MP1 Distribution Package