This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Warning_white.png (64 × 64 pixels, file size: 1 KB, MIME type: image/png)
File history
Click on a date/time to view the file as it appeared at that time.
Date/Time | Thumbnail | Dimensions | User | Comment | |
---|---|---|---|---|---|
current | 15:56, 7 October 2021 | 64 × 64 (1 KB) | Registered User | Merge articles upload |
You cannot overwrite this file.
File usage
More than 100 pages use this file. The following list shows the first 100 pages that use this file only. A full list is available.
- ADC device tree configuration
- Audio codecs hardware components
- Boot chains overview
- CEC device tree configuration
- CRC device tree configuration
- CRYP device tree configuration
- Clock device tree configuration
- Cross-compile with OpenSTLinux SDK
- DAC device tree configuration
- DCMI device tree configuration
- DFSDM device tree configuration
- DMAMUX device tree configuration
- DMA device tree configuration
- DSI device tree configuration
- Debugging the Linux kernel using the GDB
- Development setup for STM32MPU Embedded Software
- Dmesg and Linux kernel log
- Ethernet device tree configuration
- FDCAN device tree configuration
- FMC device tree configuration
- Ftrace
- GDB
- GPIO device tree configuration
- GPU device tree configuration
- Gdbgui
- HASH device tree configuration
- How to add a customer application
- How to create your own image
- How to create your own machine
- How to cross-compile with the Developer Package
- How to customize the Linux kernel
- How to display on HDMI
- How to launch Khronos OpenGLES conformance tests
- How to launch glmark2 benchmark
- How to set up a SocketCAN interface
- How to use the kernel dynamic debug
- I2C device tree configuration
- I2C i2c-tools
- IWDG device tree configuration
- Ifconfig
- Kmemleak
- LEDs and buttons on STM32 MPU boards
- LPTIM device tree configuration
- LTDC device tree configuration
- Linux remoteproc framework overview
- MDMA device tree configuration
- NVMEM overview
- OTG device tree configuration
- OpenEmbedded - devtool
- PC prerequisites
- Pinctrl device tree configuration
- QUADSPI device tree configuration
- RNG device tree configuration
- SAI device tree configuration
- SDMMC device tree configuration
- SDMMC internal peripheral
- SPDIFRX Linux driver
- SPDIFRX device tree configuration
- STM32CubeProgrammer
- STM32CubeProgrammer flashlayout
- STM32MP157C-EV1 - board assembly
- STM32MP157C-EV1 - board connections
- STM32MP157C-EV1 - hardware description
- STM32MP157X-DKX - board connections
- STM32MP157X-DKX - hardware description
- STM32MP157x-DKx - board assembly
- STM32MP15 Discovery kits - Starter Package
- STM32MP15 Discovery kits - required material
- STM32MP15 Discovery kits - starting for the first time
- STM32MP15 Evaluation boards - Starter Package
- STM32MP15 Evaluation boards - required material
- STM32MP15 Evaluation boards - starting for the first time
- STM32MP15 TF-A
- STM32MP15 U-Boot
- STM32MP15 backup registers
- STM32MP1 Developer Package
- STM32MP1 Developer Package - Linux kernel
- STM32MP1 Developer Package - SDK
- STM32MP1 Developer Package - STM32CubeMP1 Package
- STM32MP1 Developer Package - TF-A
- STM32MP1 Developer Package - U-Boot
- STM32MP1 Developer Package - debug symbol files
- STM32MP1 Distribution Package
- STM32MP1 Distribution Package - OpenSTLinux distribution
- STM32MP1 Starter Package - images
- Serial TTY device tree configuration
- Soundcard configuration
- Subpart - STM32MP15 - Starter Package
- Sysprof
- TAMP internal peripheral
- TF-A - How to debug
- TIM device tree configuration
- U-Boot overview
- USBH device tree configuration
- USBPHYC device tree configuration
- WLAN device tree configuration
- Yavta
- Template:Green
- Template:Grey
- Template:Warning
View more links to this file.