Modify, rebuild and reload the Linux® kernel

Revision as of 17:51, 14 December 2023 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


1. Overview[edit source]

This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then you will execute step by step procedures to modify, rebuild and reload the Linux® kernel.

2. Download OpenSTLinux BSP that includes the Linux® kernel source code[edit source]

2.1. For STM32MP1 series[edit source]


The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

  • The OpenSTLinux BSP package is delivered through a tarball file named en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz for STM32MP157x-EV1 More info green.png, STM32MP157x-DKx More info green.png and STM32MP135x-DK More info green.png boards.

  • Download and install the STM32MP1 OpenSTLinux BSP package.
STM32MP1 Developer Package - STM32MP1 ecosystem v5.1.0 release
Download
  • Go on st.com to download the STM32MP1 Developer Package, en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz file.
Installation
cd <working directory path>/Developer-Package
tar xvf en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Release note

Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note.

Archive box.png For information on older releases, go to Archives.


2.2. For STM32MP2 series[edit source]

STM32MPU Developer Package - OpenSTLinux BSP


3. Prepare the Linux® kernel source code[edit source]

 cd stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0

Extract the Linux® kernel source

 tar xvf linux-6.1.82.tar.xz


Apply ST patches

 cd linux-6.1.82
 for p in `ls -1 ../*.patch`; do patch -p1 < $p; done


3.1. For STM32MP1 series[edit source]

Apply fragments

 make ARCH=arm multi_v7_defconfig "fragment*.config"
 for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done
 yes '' | make ARCH=arm oldconfig

3.2. For STM32MP2 series[edit source]

Apply fragments

 make defconfig fragment*.config
 for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done
 (yes '' || true) | make oldconfig

Prepare external device tree source needed to build linux

 cd ../../external-dt-v5.0-stm32mp-r1-c11-r0/
 tar xf external-dt-v5.0-stm32mp-r1-c11-r0.tar.xz

To enable use of external device tree source code for other component, you must set the EXTDT_DIR variable to your shell environment

  export EXTDT_DIR=$PWD/external-dt-v5.0-stm32mp-r1-c11

Return into linux directory

 cd $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0/linux-6.1.82


4. Build the Linux® kernel source code for the first time[edit source]

4.1. For STM32MP1 series[edit source]

Info white.png Information
Building the kernel for the first time can take several minutes.
  • Build kernel images (uImage and vmlinux) and device tree (dtbs)
 make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
  • Build kernel module
 make ARCH=arm modules
  • Generate output build artifacts
 mkdir -p $PWD/install_artifact/
 make ARCH=arm INSTALL_MOD_PATH="$PWD/install_artifact" modules_install

4.2. For STM32MP2 series[edit source]

Info white.png Information
Building the kernel for the first time can take several minutes.
  • Build kernel images (uImage and vmlinux) and device tree (dtbs)
 make Image.gz vmlinux dtbs LOADADDR=0xC2000040 KBUILD_EXTDTS="${EXTDT_DIR}/linux"
 make modules
  • Generate output build artifacts
 make INSTALL_MOD_PATH="$PWD/install_artifact" modules_install
 mkdir -p $PWD/install_artifact/boot/
 cp $PWD/arch/$ARCH/boot/Image.gz $PWD/install_artifact/boot/
 cp $PWD/arch/$ARCH/boot/dts/st/st*.dtb $PWD/install_artifact/boot/


5. Deploy the Linux® kernel on the board[edit source]

5.1. For STM32MP1 series[edit source]

5.1.1. Push the Linux® kernel onto the board[edit source]

 scp arch/arm/boot/uImage root@<board ip address>:/boot

5.1.2. Push the devicetree into the board[edit source]

 scp arch/arm/boot/dts/stm32mp1xx*.dtb root@<board ip address>:/boot

5.1.3. Push the kernel modules onto the board[edit source]

  • Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
 rm install_artifact/lib/modules/6.1.28/build install_artifact/lib/modules/6.1.28/source 
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
 find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
  • Copy kernel modules
 scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
  • Using the Linux® console, regenerate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
 /sbin/depmod -a
  • Synchronize data on disk with memory
 sync

5.1.4. Reboot the board[edit source]

 reboot

5.2. For STM32MP2 series[edit source]

5.2.1. Push the Linux® kernel + devicetree onto the board[edit source]

 cd install_artifact/
 scp -r boot/* root@<ip of board>:/boot/

5.2.2. Push the kernel modules onto the board[edit source]

  • Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
 rm lib/modules/6.1.28/source lib/modules/6.1.28/build
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
 find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates 
  • Copy kernel modules
 scp -r lib/modules/* root@<ip of board>:/lib/modules/
  • Generate a list of module dependencies (modules.dep) and a list of symbols provided by modules (modules.symbols):
 ssh root@<ip of board> /sbin/depmod -a
  • Synchronize data on disk with memory
 ssh root@<ip of board> sync

5.2.3. Reboot the board in order to take update into account[edit source]

 ssh root@<ip of board> reboot


6. Modify a built-in Linux® kernel device driver[edit source]

This simple example adds unconditional log information when the display driver is probed.

  • Using the Linux® console, check that there is no log information when the display driver is probed
 dmesg | grep -i stm_drm_platform_probe

  • Go to the Linux® kernel source directory
 cd $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0/linux-6.1.82

  • Edit the ./drivers/gpu/drm/stm/drv.c source file
  • Add a log information in the stm_drm_platform_probe function as follows
static int stm_drm_platform_probe(struct platform_device *pdev)
{
	struct device *dev = &pdev->dev;
	struct drm_device *ddev;
	int ret;
	[...]

	DRM_INFO("Simple example - %s\n", __func__);

	return 0;
	[...]
}
  • Save the file

6.1. For STM32MP1 series[edit source]

  • Rebuild the Linux® kernel
 make uImage LOADADDR=0xC2000040
  • Update the Linux kernel image into board
 scp arch/arm/boot/uImage root@<board ip address>:/boot
  • Reboot the board
 reboot
  • Check that log information is now present when the display driver is probed
 dmesg | grep -i stm_drm_platform_probe
[    2.764080] [drm] Simple example - stm_drm_platform_probe

6.2. For STM32MP2 series[edit source]

  • Rebuild the Linux® kernel
 make Image.gz vmlinux LOADADDR=0xC2000040
  • Update the Linux kernel image into board
 scp arch/arm64/boot/Image.gz root@<ip of board>:/boot
  • Reboot the board
 ssh root@<ip of board> reboot
  • Check that log information is now present when the display driver is probed
 dmesg | grep -i stm_drm_platform_probe
[    2.764080] [drm] Simple example - stm_drm_platform_probe


7. STM32MP257F-EV1 Evaluation board More info green.png with OSTL device tree[edit source]

For compilation of OSTL device tree in the external Git, linux/stm32mp257f-ev1-ca35tdcid-ostl.dts , you can add this git inside Linux® kernel tree or outside Linux® kernel tree.

7.1. External git inside Linux® kernel tree[edit source]

  git submodule add https://github.com/STMicroelectronics/dt-stm32mp arch/arm64/boot/dts/st/external-dt
  make  dtbs
 or
  make  stm32mp257f-ev1-ca35tdcid-ostl.dtb

7.2. External git outside Linux® kernel tree with KBUILD_EXTDTS[edit source]

  git clone https://github.com/STMicroelectronics/dt-stm32mp ../dt-stm32mp
  make dtbs KBUILD_EXTDTS=$PATH/dt-stm32mp
 or
  make stm32mp257f-ev1-ca35tdcid-ostl.dtb KBUILD_EXTDTS=$PATH/dt-stm32mp