This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
Line 7: | Line 7: | ||
</noinclude> | </noinclude> | ||
{|class=" | {|class="contenttable" style="text-align:left; border-style:solid; border-color:#00C0FF; background:white;" width="95%" cellspacing="1" | ||
|- | |- | ||
! colspan="2" style="text-align:left; border-color:#00C0FF; background:#00C0FF; color:white;" valign="top" | '''STM32MP1 Platform trace and debug environment'''<br><br> ''Which software and/or hardware component(s) can be monitored, traced or debugged, and how? <br> What are the possible tracing, monitoring and debugging paths? '' <br><br> {{highlight|Click on the links in the frame below and be guided!}} | ! colspan="2" style="text-align:left; border-color:#00C0FF; background:#00C0FF; color:white;" valign="top" | '''STM32MP1 Platform trace and debug environment'''<br><br> ''Which software and/or hardware component(s) can be monitored, traced or debugged, and how? <br> What are the possible tracing, monitoring and debugging paths? '' <br><br> {{highlight|Click on the links in the frame below and be guided!}} |
Revision as of 17:55, 12 February 2019
Template:ArticleApprovedVersion
STM32MP1 Platform trace and debug environment Which software and/or hardware component(s) can be monitored, traced or debugged, and how? What are the possible tracing, monitoring and debugging paths? Click on the links in the frame below and be guided! | |
---|---|
![]() STM32MP1 Platform trace and debug environment overview |
![]() STM32MP1 Platform trace and debug environment overview for Android |
You can also find articles related to the "Trace and debug tools" item by browsing through the category tree below: