This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Page title matches
- 9 KB (1,389 words) - 15:53, 12 April 2024
Page text matches
- This article explains what SPI is and uses examples to demonstrate how to use it. ==What is Serial Peripheral Interface (SPI)?== Serial Peripheral ...9 KB (1,389 words) - 15:53, 12 April 2024
- * NOR Flash memories (SPI/Quad-SPI/Octo-SPI), making use of wear-levelling ... h” file. The LevelX driver Octo-SPI header template file below ...5 KB (716 words) - 13:54, 7 June 2022
- lines between the STM32 and an external Quad-SPI memory. This interface supports ... lines between the STM32 and an external Octo-SPI memory. This interface supports ...12 KB (1,655 words) - 11:46, 26 September 2024
- through a standard serial interface, e.g. UART, SPI. The host can send ... a standard serial interface, e.g. UART, SPI. A specific applciation interface ...29 KB (4,693 words) - 14:08, 28 September 2024
- bootloader interface (UART, USB DFU, I2C, SPI, and CAN). ... | SPI || -c port=SPI br=375 cpha=1edge cpol=low |- | CAN || -c port ...6 KB (957 words) - 09:52, 26 April 2023
- * Getting started with Octo-SPI and Hexadeca-SPI Interface on STM32microcon ... * Select Octo SPI mode . * Select the Port and the Chip Select. ...11 KB (1,663 words) - 11:10, 10 September 2024
- for toggling GPIO at 1 Hz, while using SPI at 45 MHz requires very high ... is important for faster peripherals such as SPI or USART. ...5 KB (732 words) - 16:49, 26 December 2022
- __NOTOC__ Learn how to use STM32 features with simple examples ==System peripherals== {|class="contenttable" style="margin: auto; ...5 KB (703 words) - 10:25, 23 August 2024
- through communication interface such as I2C or SPI), when the device is in Stop 2 mode. A wake-up source can be any of the peripheral interrupts ...3 KB (457 words) - 10:30, 12 April 2023
- * [https://www.st.com/resource/en/application_note/dm00081379-spi ... (such as USART, CAN, FD-CAN, USB-DFU, I2C, SPI, I3C). A communication ...54 KB (8,055 words) - 10:05, 30 November 2021