This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Page title matches
File:SPI ico.png (768 × 733 (8 KB)) - 15:16, 7 May 2020File:SPI HW Connection.png (815 × 232 (18 KB)) - 16:00, 21 July 2023File:SPI Code Sequence.png (711 × 728 (51 KB)) - 16:00, 21 July 2023File:SPI Synchronization Frame.png (864 × 219 (21 KB)) - 16:00, 21 July 2023File:SPI Command Frame.png (925 × 220 (27 KB)) - 16:00, 21 July 2023File:SPI Read Data Frame.png (755 × 241 (20 KB)) - 16:00, 21 July 2023- 9 KB (1,389 words) - 15:53, 12 April 2024
File:SPI1 selection.png (1,380 × 624 (118 KB)) - 16:57, 26 January 2023File:SPI NVIC settings.png (804 × 177 (11 KB)) - 12:20, 27 January 2023File:SPI DMA settings add.png (2,778 × 1,631 (297 KB)) - 15:38, 27 January 2023File:RM0351 SPI schematic.png (2,160 × 731 (105 KB)) - 17:20, 17 February 2023File:SPI parameters master v1.png (2,128 × 2,194 (1.32 MB)) - 17:25, 17 February 2023File:SPI GPIO settings v0.png (803 × 289 (21 KB)) - 17:30, 17 February 2023File:SPI DMA SPI1 TX.png (2,587 × 2,051 (978 KB)) - 17:34, 17 February 2023File:SPI connections.png (1,000 × 581 (597 KB)) - 10:24, 9 March 2023File:I2C-SPI transfer.png (1,014 × 400 (166 KB)) - 17:53, 2 March 2023File:Ext Mem OctoSPI.png (1,291 × 1,151 (106 KB)) - 14:40, 10 July 2023File:STM32 MC spinning direction question.png (1,624 × 1,032 (172 KB)) - 14:14, 18 December 2023File:xspi2.png (452 × 832 (88 KB)) - 12:04, 8 January 2024File:xspi3.png (1,432 × 863 (260 KB)) - 14:58, 8 January 2024
Page text matches
- This article explains what SPI is and uses examples to demonstrate how to use it. ==What is Serial Peripheral Interface (SPI)?== Serial Peripheral ...9 KB (1,389 words) - 15:53, 12 April 2024
- * NOR Flash memories (SPI/Quad-SPI/Octo-SPI), making use of wear-levelling ... h” file. The LevelX driver Octo-SPI header template file below ...5 KB (716 words) - 13:54, 7 June 2022
- bootloader interface (UART, USB DFU, I2C, SPI, and CAN). ... | SPI || -c port=SPI br=375 cpha=1edge cpol=low |- | CAN || -c port ...6 KB (957 words) - 09:52, 26 April 2023
- * Getting started with Octo-SPI and Hexadeca-SPI Interface on STM32microcon ... * Select Octo SPI mode . * Select the Port and the Chip Select. ...11 KB (1,677 words) - 13:41, 29 May 2024
- for toggling GPIO at 1 Hz, while using SPI at 45 MHz requires very high ... is important for faster peripherals such as SPI or USART. ...5 KB (732 words) - 16:49, 26 December 2022
- __NOTOC__ Learn how to use STM32 features with simple examples ==System peripherals== {|class="contenttable" style="margin: auto; ...5 KB (643 words) - 16:03, 12 April 2024
- through communication interface such as I2C or SPI), when the device is in Stop 2 mode. A wake-up source can be any of the peripheral interrupts ...3 KB (457 words) - 10:30, 12 April 2023
- * [https://www.st.com/resource/en/application_note/dm00081379-spi ... (such as USART, CAN, FD-CAN, USB-DFU, I2C, SPI, I3C). A communication ...54 KB (8,055 words) - 10:05, 30 November 2021
- * NOR/NAND Flash memories:(via SPI/QSPI/OSPI/FMC). In order to support ... * NOR Flash Octo-SPI interface: #define LX_NOR_OSPI_DRIVER ...27 KB (3,698 words) - 14:38, 7 June 2022
- ==How to use LPBAM for I2C or SPI transfer == like a MEM sensor for example over I2C or SPI. LPBAM and LPDMA can be used ...26 KB (4,059 words) - 12:50, 21 February 2024