Last edited 3 months ago

X-LINUX-ISP OpenSTLinux Expansion Package

Applicable for STM32MP21x lines, STM32MP25x lines



1. What is X-LINUX-ISP?[edit | edit source]

X-LINUX-ISP is a free-of-charge open-source software package providing Image Signal Processing (ISP) image quality software. It targets the STM32MP25xx and STM32MP21xx microprocessors in the STM32MP2 series that embed an ISP camera pipeline called DCMIPP.
It brings advanced image quality capabilities for developers working with OpenSTLinux to create an ISP-based application very easily.

  • Pre-integrated into Linux® the distributions based on ST environment
  • libcamera included, with the support of the DCMIPP ISP Image Processing Algorithm (IPA) integrating Auto Exposure (AE), Auto White Balance (AWB), and all ISP controls
  • libcamerasrc gstreamer plugin included, supporting DCMIPP ISP properties
  • Sensor tuning application included, to access the ISP configuration and perform a sensor tuning procedure; it runs on the target and interacts with the STM32 ISP IQTune desktop application executed on the host computer (connected through USB)
  • Simple ISP preview application example included, taking advantage of libcamera and libcamerasrc gstreamer plugin for easy prototyping
  • Delivered under GitHub as a Yocto meta-layer



2. X-LINUX-ISP v6.2.0[edit | edit source]

Information
This version is compatible with Yocto Project® build system Scarthgap (v5.0.17). It has been validated against the OpenSTLinux ecosystem release v6.2.1 and STM32MP2 series' boards .

2.1. Contents[edit | edit source]

  • ISP frameworks:
    • libcamera based on v0.3.0 with the support of the DCMIPP ISP Image Processing Algorithm (IPA), integrating Auto Exposure (AE), Auto White Balance (AWB), and all ISP controls
    • GStreamer libcamerasrc plugin based on v0.3.0 with the support of DCMIPP ISP properties
  • Supported image sensors:
    • Sony IMX335 (5MP)
    • Framework ready to support customer image sensors

2.2. Validated hardware[edit | edit source]

X-LINUX-ISP v6.2.0 supports STM32MP2 series' boards ; it has been validated on the following board:

  • STM32MP257F-EV1 Evaluation board
  • STM32MP257F-DK Discovery kit
  • STM32MP215F-DK Discovery kit


3. X-LINUX-ISP package[edit | edit source]

X-LINUX-ISP Starter package

X-LINUX-ISP Starter package

Quickly and easily bring ISP advanced image quality on STM32MP25xx microprocessors

X-LINUX-ISP Distribution package

X-LINUX-ISP Distribution package
OpenEmbedded meta-layer to be added on top of the STM32MP25xx Distribution Package to generate ISP packages







Information
A Developper Package is not delivered for the X-LINUX-ISP Expansion Package. The OpenSTLinux Developper Package is sufficient.

4. Next steps...[edit | edit source]

How to articles

How to articles

X-LINUX-ISP How to articles.

Tools

ISP - Tools

Articles dedicated to use the different X-LINUX-ISP tools