This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article aims at giving the following information:
- How to get the latest OP-TEE, TF-A, U-Boot, Linux® kernel, gcnano-driver and debug symbols for the STM32 microprocessor series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP1 ecosystem v5.0.0 release[edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
- The OpenSTLinux BSP package is delivered through a tarball file named en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz for STM32MP157x-EV1 , STM32MP157x-DKx and STM32MP135x-DK boards.
- Download and install the STM32MP1 OpenSTLinux BSP package.
STM32MP1 Developer Package - STM32MP1 ecosystem v5.0.0 release | |
---|---|
Download |
|
Installation |
cd <working directory path>/Developer-Package
tar xvf en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz |
Release note |
Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note. For information on older releases, go to Archives. |
- In the <Developer Package installation directory>/stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/, a tarball archive of the OpenSTLinux BSP components can be found.
- The Linux kernel installation directory is named linux-stm32mp-<kernel version>:
linux-stm32mp-6.1.28-stm32mp-r1-r0 Linux kernel installation directory ├── [*].patch ST patches to apply during the Linux kernel preparation (see next chapter) ├── fragment-[*].config ST configuration fragments to apply during the Linux kernel configuration (see next chapter) ├── optional-fragment-[*].config Optional ST configuration fragments to apply during the Linux kernel configuration depending on your needs (SMP or not, signature or not, ...) ├── linux-6.1.28.tar.xz Tarball file of the Linux kernel source code ├── README.HOW_TO.txt Helper file for Linux kernel management: reference for Linux kernel build └── series List of all ST patches to apply
- The gcnano driver installation directory is named gcnano-driver-stm32mp-<gcnano driver version>:
gcnano-driver-stm32mp-6.4.13-stm32mp-r1-r0 gcnano-driver installation directory ├── gcnano-driver-stm32mp-6.4.13-stm32mp-r1-r0.tar.xz Tarball file of the gcnano-driver source code └── README.HOW_TO.txt Helper file for gcnano-driver management: reference for gcnano-driver build
- The U-Boot installation directory is named u-boot-stm32mp-<U-Boot version>:
u-boot-stm32mp-v2022.10-stm32mp-r1-r0 U-Boot installation directory ├── [*].patch ST patches to apply during the U-Boot preparation (see next chapter) ├── u-boot-stm32mp-v2022.10-stm32mp-r1 U-Boot source code directory ├── Makefile.sdk Makefile for the U-Boot compilation ├── README.HOW_TO.txt Helper file for U-Boot management: reference for U-Boot build ├── series List of all ST patches to apply └── u-boot-stm32mp-v2022.10-stm32mp-r1-r0.tar.xz Tarball file of the U-Boot source code
- The TF-A installation directory is named tf-a-stm32mp-<TF-A version>:
tf-a-stm32mp-v2.8.6-stm32mp-r1-r0 TF-A installation directory ├── [*].patch ST patches to apply during the TF-A preparation (see next chapter) ├── tf-a-stm32mp-v2.8.6-stm32mp-r1 TF-A source code directory ├── Makefile.sdk Makefile for the TF-A compilation ├── README.HOW_TO.txt Helper file for TF-A management: reference for TF-A build ├── series List of all ST patches to apply └── tf-a-stm32mp-v2.8.6-stm32mp-r1-r0.tar.xz Tarball file of the TF-A source code
- The OP-TEE installation directory is named optee-os-stm32mp-<OP-TEE version>:
optee-os-stm32mp-3.19.0-stm32mp-r1-r0 OP-TEE installation directory ├── [*].patch ST patches to apply during the OP-TEE preparation (see next chapter) ├── optee-os-stm32mp-3.19.0-stm32mp-r1 OP-TEE source code directory ├── fonts.tar.gz fonts for OPTEE-OS ├── Makefile.sdk Makefile for the OP-TEE compilation ├── optee-os-stm32mp-3.19.0-stm32mp-r1-r0.tar.xz Tarball file of the OP-TEE source code ├── README.HOW_TO.txt Helper file for OP-TEE management: reference for OP-TEE build └── series List of all ST patches to apply
- The FIP artifacts directory is named FIP_artifacts:
FIP_artifacts ├── arm-trusted-firmware │ ├── fwconfig │ │ ├── stm32mp13[*]-fw-config-optee.dtb Device tree for FW config → STM32MP13 boards │ │ └── stm32mp15[*]-fw-config-optee.dtb Device tree for FW config → STM32MP15 boards │ ├── metada.bin Store boot information │ ├── tf-a-stm32mp13[*].stm32 FSBL binary→ STM32MP13 boards │ └── tf-a-stm32mp15[*].stm32 FSBL binary → STM32MP15 boards ├── optee │ ├── tee-header_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ ├── tee-header_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 kits │ ├── tee-pageable_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ ├── tee-pageable_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 boards │ ├── tee-pager_v2-stm32mp13[*].bin Binary file for OP-TEE OS → STM32MP13 boards │ └── tee-pager_v2-stm32mp15[*].bin Binary file for OP-TEE OS → STM32MP15 boards └── u-boot ├── u-boot-nodtb-stm32mp13.bin ├── u-boot-nodtb-stm32mp15.bin ├── u-boot-stm32mp13[*].dtb Device tree for U-Boot → STM32MP13 boards └── u-boot-stm32mp15[*].dtb Device tree for U-Boot → STM32MP15 boards
- The debug symbol files are located under the <Developer Package installation directory>/stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/images/stm32mp1 directory:
2. Archives [edit source]
This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.