"Revision ID" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage2628previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.SSTM32MP15 Discovery kits - starting for the first time +100852 +STM32MP15 Evaluation boards +90186 +STM32MP15 Evaluation boards - Starter Package +104904 +STM32MP15 Evaluation boards - required material +100836 +STM32MP15 Evaluation boards - starting for the first time +100837 +STM32MP15 Linux kernel overview +90329 +STM32MP15 Linux kernel.png +82587 +STM32MP15 MCU SRAM internal memory +100562 +STM32MP15 OP-TEE overview +106552 +STM32MP15 OP-TEE overview.png +106549 +STM32MP15 OTP mapping +102176 +STM32MP15 PWR internal peripheral +104052 +STM32MP15 RAM mapping +90510 +STM32MP15 U-Boot +95117 +STM32MP15 V4L2 camera overview +97234 +STM32MP15 VREFBUF internal peripheral +100564 +STM32MP15 backup registers +101421 +STM32MP15 boards +93994 +STM32MP15 boot information 1.png +41023 +STM32MP15 boot information 2.png +41024 +