The number of approved revisions in the page history This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage2452previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.SSTM32MP13 ADC internal peripheral +5 +STM32MP13 Developer Package - STM32CubeMP13 Package +2 +STM32MP13 Discovery kits +2 +STM32MP13 Discovery kits - Starter Package +9 +STM32MP13 Discovery kits - required material +6 +STM32MP13 Discovery kits - starting for the first time +4 +STM32MP13 Linux kernel overview +3 +STM32MP13 Linux kernel.png +2 +STM32MP13 OP-TEE overview +1 +STM32MP13 OP-TEE overview.png +0 +STM32MP13 OTP mapping +7 +STM32MP13 PWR internal peripheral +8 +STM32MP13 Package Structure.png +1 +STM32MP13 RAM mapping +2 +STM32MP13 SRAM internal memory +4 +STM32MP13 Software memory mapping.png +1 +STM32MP13 U-Boot +11 +STM32MP13 V4L2 camera overview +13 +STM32MP13 VREFBUF internal peripheral +7 +STM32MP13 backup registers +7 +