This article proposes to address the creation of a simple hello-world application with STM32CubeIDE.
1. Create a GtkHelloWorld user space project[edit source]
In Cortex®-A7 sub-project context, named here MP157C-DK2_CA7, right-click and select Create a userspace Project...
![User space project wizard shortcut User space project wizard shortcut](/stm32mpu/nsfr_img_auth.php/8/8d/UserSpaceShortCut.png)
Here, an Executable project type in C language is selected. Note that the user space project uses by default the SDK version associated to the Cortex®-A7 sub-project.
![User space project creation wizard' User space project creation wizard'](/stm32mpu/nsfr_img_auth.php/b/b6/CubeIDEUserSpaceGtkCreation.png)
Below, the main.c source code is updated with gtk_hello_world.c as defined in article Create a simple hello-world application.
2. Update GtkHelloWorld project sources and properties[edit source]
The proposal to reference the Gtk library is to use the pkg-config command to update the compiler and linker flags, just like it is done in the Makefile of article Create a simple hello-world application. This properties update is done inside menu GtkHelloWorld properties: C/C++ Build > Settings > Tool Settings.
- main.c update and C flag: `pkg-config --cflags gtk+-3.0`
![GtkHelloWorld project source & properties update GtkHelloWorld project source & properties update](/stm32mpu/nsfr_img_auth.php/0/0d/CubeIDEUserSpaceGtkBuildSetup.png)
- Linker flags update: `pkg-config --libs gtk+-3.0`
![GtkHelloWorld project source & properties update GtkHelloWorld project source & properties update](/stm32mpu/nsfr_img_auth.php/6/6c/CubeIDEUserSpaceGtkBuildSetup2.png)
- Now build GtKHelloWorld project by right-clicking on it and then Build Project.
![GtkHelloWorld project source & properties update GtkHelloWorld project source & properties update](/stm32mpu/nsfr_img_auth.php/f/fb/CubeIDEUserSpaceGtkBuild.png)
3. Prepare Debug Configuration[edit source]
You can check boot messages via Linux® console opened with butterfly icon (shown below), but remember this console cannot be shared outside STM32CubeIDE (minicom,...). In order to debug user space application, your target must be Linux® booted and network connected.
In order to check network connection, start the Target Status widget in the bottom right corner of the window.
Check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.
4. Debug Configuration[edit source]
- Select your project, right-click Debug as... > Debug Configurations,
- then select STM32 Cortex-A Remote Application'.
![Debug configuration shortcut Debug configuration shortcut](/stm32mpu/nsfr_img_auth.php/2/27/CubeIDEUserSpaceDebugShortCut.png)
In the Main tab, select connection "MPU SSH Weston", corresponding to the target IP address discovered by the Target Status widget, it's destination directory is /home/weston.
![Debug setup Debug setup](/stm32mpu/nsfr_img_auth.php/f/f3/CubeIDEUserSpaceGtkDebugSetup.png)
5. Debug[edit source]
Click Debug :
- GtkHelloWorld is downloaded to the target,
- GDBServer is launched on the target,
- GDBClient is launched on the workstation and can exchange via the network with GDBServer.
![GtkHelloWorld debug GtkHelloWorld debug](/stm32mpu/nsfr_img_auth.php/4/41/CubeIDEUserSpaceGtkDebug.png)