This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to File:Warning white.png:
Displayed 50 items.
- SAI device tree configuration (file link) (← links)
- Soundcard configuration (file link) (← links)
- Serial TTY device tree configuration (file link) (← links)
- STM32MP157x-DKx - board connections (file link) (← links)
- STM32MP15 Discovery kits - starting for the first time (file link) (← links)
- STM32MP157x-DKx - board assembly (file link) (← links)
- STM32MP157x-DKx - hardware description (file link) (← links)
- STM32MP15 Discovery kits - required material (file link) (← links)
- STM32MP15 Discovery kits - Starter Package (file link) (← links)
- USBH device tree configuration (file link) (← links)
- I2C device tree configuration (file link) (← links)
- OTG device tree configuration (file link) (← links)
- How to create your own machine (file link) (← links)
- How to create your own image (file link) (← links)
- SPDIFRX Linux driver (file link) (← links)
- DMAMUX device tree configuration (file link) (← links)
- DMA device tree configuration (file link) (← links)
- MDMA device tree configuration (file link) (← links)
- DAC device tree configuration (file link) (← links)
- Debugging the Linux kernel using the GDB (file link) (← links)
- RNG device tree configuration (file link) (← links)
- CRYP device tree configuration (file link) (← links)
- CRC device tree configuration (file link) (← links)
- HASH device tree configuration (file link) (← links)
- How to add a customer application (file link) (← links)
- WLAN device tree configuration (file link) (← links)
- How to customize the Linux kernel (file link) (← links)
- SPDIFRX device tree configuration (file link) (← links)
- DFSDM device tree configuration (file link) (← links)
- Ethernet device tree configuration (file link) (← links)
- NVMEM overview (file link) (← links)
- IWDG device tree configuration (file link) (← links)
- USBPHYC device tree configuration (file link) (← links)
- STM32MP1 Developer Package - debug symbol files (file link) (← links)
- LEDs and buttons on STM32 MPU boards (file link) (← links)
- STM32MP15 backup registers (file link) (← links)
- LTDC device tree configuration (file link) (← links)
- CEC device tree configuration (file link) (← links)
- GPU device tree configuration (file link) (← links)
- DSI device tree configuration (file link) (← links)
- DCMI device tree configuration (file link) (← links)
- FDCAN device tree configuration (file link) (← links)
- How to set up a SocketCAN interface (file link) (← links)
- How to configure ethernet interface (file link) (← links)
- How to profile video framerate (file link) (← links)
- How to play audio (file link) (← links)
- STM32MP15 ROM code overview (file link) (← links)
- STM32CubeMP1 Package (file link) (← links)
- SPI overview (file link) (← links)
- STM32MP15 secure boot (file link) (← links)