This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Board$:
Displayed 50 items.
- DFSDM Linux driver (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to update U-Boot on an SD card (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- Configfs (transclusion) (← links)
- How to configure a wlan interface on hotspot mode (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- How to set up a Bluetooth connection (transclusion) (← links)
- How to scan Bluetooth devices (transclusion) (← links)
- How to scan BLE devices (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- How to monitor the display framerate (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to control a RNG in userspace (transclusion) (← links)
- How to retrieve Cortex-M4 logs after crash (transclusion) (← links)
- How to monitor the GCNANO GPU load (transclusion) (← links)
- DRM KMS troubleshooting grid (transclusion) (← links)
- How to play audio (transclusion) (← links)
- Reading tips (transclusion) (← links)
- Debugfs (transclusion) (← links)
- STM32CubeMP1 Package (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)
- How to cross-compile with the Distribution Package (transclusion) (← links)
- HDP Linux driver (transclusion) (← links)
- DRM KMS overview (transclusion) (← links)
- STM32MP15 secure boot (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157C-DK2/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157C-DK2/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157C-DK2/Develop on Arm® Cortex®-A7/Modify, rebuild and reload the Linux® kernel (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157C-DK2/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- How to start the coprocessor from the bootloader (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7/Modify, rebuild and reload the Linux® kernel (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- STM32MP15 Evaluation boards - Starter Package for Android (transclusion) (← links)
- STM32MP1 Developer Package for Android (transclusion) (← links)
- Create a simple hello-world application (transclusion) (← links)
- Modify, rebuild and reload the Linux® kernel (transclusion) (← links)
- How to accelerate JPEG compression and decompression (transclusion) (← links)