Approved version. Approved on: 13:05, 22 October 2019
You are viewing an old version of this page. Return to the latest version.
- Last edited 3 weeks ago ago
STM32MP15 internal peripherals assignment table template
Revision as of 13:02, 13 February 2019 by Gerald Baeza (talk | contribs)
Template:ArticleMainWriter Template:ArticleApprovedVersion
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |