Information |
The following licenses are applicable to the version v5.1.0 of the X-LINUX-AZURE Expansion Package. |
1. Top software license agreement (SLA) and application licenses[edit source]
1.1. Software license agreement[edit source]
License |
---|
SLA0048 Rev4/March 2018
|
2. Software bill of materials[edit source]
List of software brought by X-LINUX-AZURE expansion package, installed on image st-image-azure in addition to image st-image-weston
Recipe Name | Package Name | Version | Copyright | License | Description |
---|---|---|---|---|---|
aziot-edged | aziot-edged | 1.4.27-r1 | Microsoft Corporation. All rights reserved. | MIT | The aziot-edged is the main binary for the IoT edge daemon. Customized by X-LINUX-AZURE. |
aziot-keys | aziot-keys | 1.4.7.0+91e058880c-r1 | Microsoft Corporation. All rights reserved. | MIT | aziot-keys is the default implementation of cryptographic operations used by the Keys Service. Customized by X-LINUX-AZURE. |
aziotctl | aziotctl | 1.4.7.0+91e058880c-r1 | Microsoft Corporation. All rights reserved. | MIT | aziotctl is used to manage the IoT Identity Service and related services. Customized by X-LINUX-AZURE. |
aziotd | aziotd | 1.4.7.0+91e058880c-r1 | Microsoft Corporation. All rights reserved. | MIT | aziotd is the main binary for the IoT Identity Service and related services. Customized by X-LINUX-AZURE. |
containerd-opencontainers | containerd-opencontainers | v1.7.1+git0+835383b17f | Docker, Inc | Apache-2.0 | containerd is a daemon to control runC |
demo-application-azure | demo-application-azure | 5.1 | STMicroelectronics | BSD-3-Clause | Add basic support of Azure IoT Edge on Demo Launcher |
docker-ce | docker-ce docker-ce-cli |
23.0.2-ce+git219f21bf07502b447095649b5a2764661737f164 | Docker, Inc | Apache-2.0 | Linux container runtime |
iotedge | iotedge | 1.4.27-r1 | Microsoft Corporation. All rights reserved. | MIT | The iotedge tool is used to manage the IoT Edge runtime. Customized by X-LINUX-AZURE. |
libseccomp | libseccomp | 2.5.4 | Red Hat <pmoore@redhat.com> Red Hat <mjuszkiewicz@redhat.com> Imagination Technologies Ltd. Helge Deller <deller@gmx.de> Freescale <bogdan.purcareata@freescale.com> IBM Microsoft Corporation. <paulmoore@microsoft.com> Cisco Systems, Inc. <pmoore2@cisco.com> |
LGPL-2.1 | interface to seccomp filtering mechanism |
pkcs11-provider | pkcs11-provider | 0.4 | simo@redhat.com | Apache-2.0 | This is an Openssl 3.x provider to access Hardware or Software Tokens using the PKCS#11 Cryptographic Token Interface |
runc-opencontainers | runc-opencontainers | 1.1.7+git0+b6109acd4d | Docker, Inc | Apache-2.0 | runc container cli tools |
tini | tini | 0.19.0 | Thomas Orozco <thomas@orozco.fr> | MIT | Minimal init for containers |
tpm2-abrmd | tpm2-abrmd | 3.0.0 | Intel Corporation | BSD-2-Clause | TPM2 Access Broker & Resource Manager |
tpm2-openssl | tpm2-openssl | 1.1.1 | Fraunhofer SIT sponsored by Infineon Technologies AG Wind River Systems Petr Gotthard |
BSD-3-Clause | Provider for integration of TPM 2.0 to OpenSSL 3.0 |
tpm2-pkcs11 | tpm2-pkcs11 | 1.9.0-r1 | g10 Code GmbH Andreas Jellinghaus Red Hat, Inc. |
BSD-2-Clause | A PKCS#11 interface for TPM2 hardware Customized by X-LINUX-AZURE. |
tpm2-tools | tpm2-tools | 5.5 | Alibaba Group Atom Software Studios, s.r.o. Emmanuel Deloget <logout@free.fr> Fraunhofer SIT Fraunhofer SIT sponsored by Infineon Technologies AG GlovePuppet Intel Corporation Massachusetts Institute of Technology National Instruments Red Hat, Inc. Sebastien LE STUM SUSE GmbH Wind River Systems |
BSD-3-Clause | Tools for TPM2. |
tpm2-totp | tpm2-totp | 0.3.0 | Behdad Esfahbod Fraunhofer SIT Jonas Witschel Linux TPM2 & TSS2 Software Red Hat Inc. |
BSD-3-Clause | Attest the trustworthiness of a device against a human using time-based one-time passwords |
tpm2-tss | tpm2-tss libtss2 libtss2-tcti-mssim0 libtss2-tcti-device0 libtss2-mu0 |
4.0.1 | Andreas Droescher Behdad Esfahbod Facebook, Inc. and its affiliates Fraunhofer SIT Fraunhofer SIT sponsored by Infineon Technologies AG Intel Intel Corporation Infineon Technologies AG Red Hat Inc. Wind River Systems |
BSD-2-Clause | Software stack for TPM2. |
tpm2-tss-engine | tpm2-tss-engine tpm2-tss-engine-engines |
1.1.0 | Fraunhofer SIT sponsored by Infineon Fraunhofer SIT sponsored by Infineon Technologies AG Wind River Systems. |
BSD-3-Clause | The tpm2-tss-engine project implements a cryptographic engine for OpenSSL. |
trousers | trousers | 0.3.15+git0+94144b0a1d | Christian Kummer TrouSerS Project International Business Machines Corp Intel Corporation |
BSD-3-Clause | TrouSerS - An open-source TCG Software Stack implementation. |
List of software brought by OpenSTLinux, needed by X-LINUX-AZURE expansion package, installed on image st-image-azure, available on ST package repository.
Recipe Name | Package Name | Version | License | Description |
---|---|---|---|---|
ccid | ccid | 1.5.2 | LGPL-2.1 | Generic USB CCID smart card reader driver |
connman | connman-client connman |
1.41 | GPL-2.0 | A daemon for managing internet connections within embedded devices |
glibc | libc6-utils | 2.37-r1 | LGPL-2.0 | Miscellaneous utilities provided by glibc |
libtasn1 | libtasn1-6 | 4.19.0 | LGPL-2.1 | Library for ASN.1 and DER manipulation |
opensc | opensc | 0.23.0 | LGPL-2.1 | Smart card library and applications |
optee-client | optee-client | 3.19.0+git0+140bf46304-r1 | BSD-2-Clause | OPTEE Client Customized by X-LINUX-AZURE. |
optee-os-stm32mp | optee-os-stm32mp-ta-pkcs11 | 3.19.0-stm32mp-r2-r1 | BSD-2-Clause | OPTEE TA development kit for stm32mp Customized by X-LINUX-AZURE. |
p11-kit | p11-kit | 0.24.1 | BSD-3-Clause | Provides a way to load and enumerate PKCS#11 modules |
pcsc-lite | pcsc-lite libpcsclite1 |
1.9.9 | BSD-3-Clause | PC/SC Lite smart card framework and applications |
run-postinsts | run-postinsts | 1.0-r10 | MIT | Runs postinstall scripts on first boot of the target device |