The number of approved revisions in the page history This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage2452previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.HHow to run use cases +1 +How to run use cases with expansions +2 +How to run use cases with expansions.png +3 +How to run use cases.png +3 +How to scan BLE devices +4 +How to scan Bluetooth devices +4 +How to send or receive CAN data +5 +How to set up a Bluetooth connection +4 +How to set up a SocketCAN interface +4 +How to set up proxy and P2P Ethernet connection with STM32CubeIDE +3 +How to setup a WLAN connection +7 +How to setup target password in STM32CubeIDE +3 +How to start the coprocessor from the bootloader +15 +How to stop and start Weston +8 +How to stream RAW camera over network +4 +How to stream camera over network +12 +How to structure the software to develop STM32Cube examples +1 +How to support EXT4 through MMC +9 +How to support UBIFS through MTD +6 +How to test and benchmark OpenGLES +5 +