![AI X-LINUX-AI-logo.png](/stm32mpu/nsfr_img_auth.php/thumb/8/87/AI_X-LINUX-AI-logo.png/700px-AI_X-LINUX-AI-logo.png)
1. What is X-LINUX-AI?[edit source]
X-LINUX-AI is a free of charge open-source software package dedicated to AI.
It is a complete ecosystem that allow developers working with OpenSTLinux to create AI-based application very easily.
- All-in-one AI solutions for the entire STM32 MPU boards
- Pre-integrated into Linux distribution based on ST environment
- Include AI frameworks to execute Neural Network models
- Include AI model benchmark application tools for MPU
- Easy application prototyping using Python language and AI frameworks Python API
- C++ API for embedded high-performance applications
- Optimized open-source solutions provided with source codes that allow extensive code reuse and time savings
- Delivered under GitHub as a Yocto meta-layer
![What is x linux ai.png](/stm32mpu/nsfr_img_auth.php/b/b5/What_is_x_linux_ai.png)
2. X-LINUX-AI Software stack introduction[edit source]
X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MPx Series devices.
It contains Linux AI frameworks, development tools, as well as application examples to get started with some basic AI use cases such as computer vision.
It is composed of an OpenEmbedded meta layer, named meta-st-x-linux-ai, to be added on top of the STM32MPx Distribution Package. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MPx Series devices.
Depending on the STM32MPU series X-LINUX-AI supports inference execution either on Neural Processing Unit (NPU), Graphics Processing Unit (GPU) or Cortex-A (with multi-threading).
![X-LINUX-AI supported inference engine VS sSTM32MPUs series X-LINUX-AI supported inference engine VS sSTM32MPUs series](/stm32mpu/nsfr_img_auth.php/2/2a/X-LINUX-AI_supported_inference_engine_vs_stm32mpu_series.png)
2.1. Seamless integration of common AI frameworks[edit source]
![X-LINUX-AI software structure.png](/stm32mpu/nsfr_img_auth.php/e/e4/X-LINUX-AI_software_structure.png)
2.2. AI framework details[edit source]
2.2.1. Tensorflow Lite runtime[edit source]
![X-LINUX-AI tflite fw details.png](/stm32mpu/nsfr_img_auth.php/thumb/a/a6/X-LINUX-AI_tflite_fw_details.png/600px-X-LINUX-AI_tflite_fw_details.png)
2.2.2. ONNX runtime[edit source]
![X-LINUX-AI Onnx fw details.png](/stm32mpu/nsfr_img_auth.php/thumb/0/0c/X-LINUX-AI_Onnx_fw_details.png/600px-X-LINUX-AI_Onnx_fw_details.png)
3. unknown revision[edit source]
3.1. Contents[edit source]
- TensorFlow™ Lite[1] 2.11.0 with XNNPACK delegate activated
- Coral Edge TPU™[2] accelerator native support
- libedgetpu 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0
- libcoral 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0
- PyCoral 2.0.0 (Grouper) aligned with TensorFlow™ Lite 2.11.0
- ONNX Runtime™ [3] 1.14.0 with XNNPACK execution engine activated
- OpenCV[4] 4.7.x
- Python™[5] 3.11.x (enabling Pillow module)
Support of Sony™ IMX335 5Mpx sensor with use of DCMIPP and internal ISP
- TensorFlow™ Lite application samples :
GPU Python human pose estimation using TensorFlow™ Lite based on Movenet SinglePose Lightning quantized model
NPU Python semantic segmentation using TensorFlow™ Lite based on DeepLabV3 quantized model
NPU C++ / Python image classification using TensorFlow™ Lite based on MobileNet v3 quantized model
NPU C++ object detection using TensorFlow™ Lite based on COCO SSD MobileNet v1 quantized model
NPU Python object detection using TensorFlow™ Lite based on Tiny YOLOv4 quantized model
NPU C++ face recognition using TensorFlow™ Lite models capable of recognizing the face of a known (enrolled) user (available on demand)
- Coral Edge TPU™ based application samples :
- C++ / Python image classification using Coral Edge TPU™ based on MobileNet v1 quantized model and compiled for the Coral Edge TPU™
- C++ / Python object detection using Coral Edge TPU™ based on COCO SSD MobileNet v1 quantized model and compiled for the Coral Edge TPU™
- ONNX Runtime™ application samples :
Python image classification using ONNX Runtime™ based on MobileNet v3 quantized model
- C++ / Python object detection using ONNX Runtime™ based on COCO SSD MobileNet v1 quantized model
- OpenVX™ based application samples :
NPU C++ image classification using Network Binary Graph based on MobileNet v3 quantized model
- Tools :
STM32AI MPU offline tool dedicated to deploy NN on the stm32mp25
NBG benchmark application
3.2. Validated hardware[edit source]
X-LINUX-AI STM32MP25 beta is supported on all STM32MP25 Series and it has been validated on the following boards:
4. X-LINUX-AI package[edit source]
X-LINUX-AI Starter package
Quickly and easily bring AI on STM32MPUs series
X-LINUX-AI Developer package
The X-LINUX-AI SDK add-on extends the OpenSTLinux SDK
with AI functionality to develop and build an AI application easily
X-LINUX-AI Distribution package
It is an OpenEmbedded meta-layer to be added on top of the STM32MPx Distribution Package to generate AI packages
5. Next steps...[edit source]
AI - Application examples
Discover the AI applications delivered in X-LINUX-AI.
How to articles
Articles dedicated to use the different X-LINUX-AI frameworks
Tools
Articles dedicated to use the different X-LINUX-AI Tools
6. Archives
[edit source]
X-LINUX-AI release | Release note |
---|---|
X-LINUX-AI v3.0.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v3-0-0 page for the v4 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.2.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package_-_v2.2.0#X-LINUX-AI_v2-2-0 page for the v4 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.1.1 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-1 page for the v3 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.1.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-0 page for the v2 ecosystem releases (in archived wiki) |
X-LINUX-AI v2.0.0 | X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-0-0 page for the v2 ecosystem releases (in archived wiki) |
7. References[edit source]