1. Top software license agreement (SLA) and application licenses[edit source]
1.1. Software license agreement[edit source]
License |
---|
SLA0048 Rev4/March 2018
|
2. Software bill of materials[edit source]
List of software brought by X-LINUX-AZURE expansion package, installed on image st-image-azure in addition to image st-image-weston
Recipe Name | Package Name | Version | Copyright | License | Description |
---|---|---|---|---|---|
aziotctl | aziotctl | 1.4.6.0+e4b08714e1-r1 | Microsoft Corporation. All rights reserved. | MIT | aziotctl is used to manage the IoT Identity Service and related services. Customized by X-LINUX-AZURE. |
aziotd | aziotd | 1.4.6.0+e4b08714e1-r1 | Microsoft Corporation. All rights reserved. | MIT | aziotd is the main binary for the IoT Identity Service and related services. Customized by X-LINUX-AZURE. |
aziot-edged | aziot-edged | 1.4.20-r1 | Microsoft Corporation. All rights reserved. | MIT | The aziot-edged is the main binary for IoT edge daemon. Customized by X-LINUX-AZURE. |
aziot-keys | aziot-keys | 1.4.6.0+e4b08714e1-r1 | Microsoft Corporation. All rights reserved. | MIT | aziot-keys is the default implementation of cryptographic operations used by the Keys Service. Customized by X-LINUX-AZURE. |
demo-application-azure | demo-application-azure | 5.1 | Add basic support of Azure IoT Edge on Demo Launcher. | BSD-3-Clause | Add basic support of Azure IoT Edge on Demo Launcher. |
docker-ce | docker-ce docker-ce-cli |
23.0.2-ce+git219f21bf07502b447095649b5a2764661737f164 | Docker, Inc | Apache-2.0 | Linux container runtime |
iotedge | iotedge | 1.4.20-r1 | Microsoft Corporation. All rights reserved. | MIT | The iotedge tool is used to manage the IoT Edge runtime. Customized by X-LINUX-AZURE. |
pkcs11-provider | pkcs11-provider | 0.4 | simo@redhat.com | Apache-2.0 | A PKCS#11 provider for OpenSSL 3.0+ |
runc-opencontainers | runc-opencontainers | 1.1.7+git0+b6109acd4d | Docker, Inc | Apache-2.0 | runc container cli tools runc is a CLI tool for spawning and running containers according to the OCI specification. |
tpm2-abrmd | tpm2-abrmd | 3.0.0 | Intel Corporation | BSD-2-Clause | TPM2 Access Broker & Resource Manager |
tpm2-pkcs11 | tpm2-pkcs11 | 1.9.0-r1 | g10 Code GmbH Andreas Jellinghaus Red Hat, Inc. |
BSD-2-Clause | A PKCS#11 interface for TPM2 hardware. Customized by X-LINUX-AZURE to store TPM2 PKCS#11 context in /etc/tpm2_pkcs11 |
tpm2-tools | tpm2-tools | 5.5 | Alibaba Group Atom Software Studios, s.r.o. Emmanuel Deloget <logout@free.fr> Fraunhofer SIT Fraunhofer SIT sponsored by Infineon Technologies AG GlovePuppet Intel Corporation Massachusetts Institute of Technology National Instruments Red Hat, Inc. Sebastien LE STUM SUSE GmbH Wind River Systems |
BSD-3-Clause | Tools for TPM2. |
tpm2-totp | tpm2-totp | 0.3.0 | Behdad Esfahbod Fraunhofer SIT Jonas Witschel Linux TPM2 & TSS2 Software Red Hat Inc. |
BSD-3-Clause | Attest the trustworthiness of a device against a human using time-based one-time passwords |
tpm2-tss-engine | tpm2-tss-engine | 1.1.0 | Fraunhofer SIT sponsored by Infineon Fraunhofer SIT sponsored by Infineon Technologies AG Wind River Systems. |
BSD-3-Clause | Cryptographic engine implementation for OpenSSL for TPM2 |
tpm2-tss | libtss2 libtss2-mu0 libtss2-tcti-device0 libtss2-tcti-mssim0 tpm2-tss |
4.0.1 | Andreas Droescher Behdad Esfahbod Facebook, Inc. and its affiliates Fraunhofer SIT Fraunhofer SIT sponsored by Infineon Technologies AG Intel Intel Corporation Infineon Technologies AG Red Hat Inc. Wind River Systems |
BSD-2-Clause | OSS implementation of the Trusted Computing Group TPM2 Software Stack |
trousers_git | trousers | 0.3.15+git0+94144b0a1d | Christian Kummer TrouSerS Project International Business Machines Corp Intel Corporation |
BSD-3-Clause | TrouSerS - An open-source Trusted Computing Group Software Stack Implementation. |
List of software brought by OpenSTLinux, needed by X-LINUX-AZURE expansion package, installed on image st-image-azure, available on ST package repository.
Recipe Name | Package Name | Version | License | Description |
---|---|---|---|---|
ccid | ccid | 1.5.2 | LGPL-2.1-or-later | Generic USB CCID smart card reader driver |
connman | connman connman_client |
1.41 | GPL-2.0-only | A daemon for managing internet connections within embedded devices |
glibc | libc6-utils | 2.37 | LGPL-2.0-or-later | Miscellaneous utilities provided by glibc including getconf, iconv, locale, gencat, ... |
opensc | opensc | 0.23.0 | LGPL-2.0-or-later | Smart card library and applications |
optee-os-stm32mp | optee-os-stm32mp-ta-pkcs11 | 3.19.0-stm32mp-r2 | BSD-2-Clause | PKCS#11 Trusted Application for OP-TEE. |
pcsc-lite | libpcsclite1 pcsc-lite |
1.9.9 | BSD-3-Clause | PC/SC Lite smart card framework and applications |