This article aims to give the following information:
- How to download and install the latest OpenSTLinux distribution for the STM32 microprocessors Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP1-Ecosystem-v4.1.0 release[edit source]
- The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision.
- The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
- The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
- Install the STM32MP1 OpenSTLinux distribution: unknown revision
STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP1-Ecosystem-4.1.0 release | |
---|---|
Installation |
cd <working directory path>/Distribution-Package
repo init -u unknown revision -b refs/tags/unknown revision Note: "ERROR 404" may appear during "repo init" command without any impact on the process
repo sync
|
Release note |
Details about the content of this software package are available in the associated STM32 MPU ecosystem release note.
|
- When installed, the OpenSTLinux Distribution Package is available with following tree structure:
Distribution-Package OpenSTLinux distribution ├── layers │ ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ ├── meta-qt5 QT5 layer for OpenEmbedded (standard) │ ├── meta-st │ │ ├── meta-st-openstlinux STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution │ │ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ │ ├── recipes-bsp │ │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── u-boot Recipes for U-Boot │ │ │ ├── recipes-extended │ │ │ │ ├── linux-examples Recipes for Linux examples for STM32 MPU devices │ │ │ │ ├── m4coredump Recipes for script to manage coredump of cortexM4 (for STM32MP15x lineslines) │ │ │ │ ├── m4projects Recipes for firmware examples for Cortex M4 (for STM32MP15x lines
lines) │ │ │ │ └── stm32mp-g0 Recipes for G0 USB firmware (for STM32MP13x lines
lines) │ │ │ ├── recipes-graphics │ │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ ├── recipes-kernel │ │ │ │ ├── linux Recipes for Linux kernel │ │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ ├── recipes-security │ │ │ │ └── optee Recipes for OPTEE │ │ │ ├── recipes-st │ │ │ │ └── images Recipes for the bootfs and userfs partitions binaries │ │ │ └── [...] │ │ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ │ └── scripts │ │ ├── envsetup.sh Environment setup script for Distribution Package │ │ └── [...] │ └── openembedded-core Core metadata for current versions of OpenEmbedded (standard)
2. Archives
[edit source]
This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.
2.1. STM32MP1-Ecosystem-v4.0.0 release[edit source]
- The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision.
- The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
- The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
- Install the STM32MP1 OpenSTLinux distribution: unknown revision
STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP1-Ecosystem-4.0.0 release | |
---|---|
Installation |
cd <working directory path>/Distribution-Package
repo init -u unknown revision -b refs/tags/unknown revision Note: "ERROR 404" may appear during "repo init" command without any impact on the process
repo sync
|
Release note |
Details about the content of this software package are available in the associated STM32 MPU ecosystem release note.
|
- When installed, the OpenSTLinux Distribution Package is available with following tree structure:
Distribution-Package OpenSTLinux distribution ├── layers │ ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ ├── meta-qt5 QT5 layer for OpenEmbedded (standard) │ ├── meta-st │ │ ├── meta-st-openstlinux STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution │ │ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ │ ├── recipes-bsp │ │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── u-boot Recipes for U-Boot │ │ │ ├── recipes-extended │ │ │ │ ├── linux-examples Recipes for Linux examples for STM32 MPU devices │ │ │ │ ├── m4coredump Recipes for script to manage coredump of cortexM4 (for STM32MP15x lineslines) │ │ │ │ ├── m4projects Recipes for firmware examples for Cortex M4 (for STM32MP15x lines
lines) │ │ │ │ └── stm32mp-g0 Recipes for G0 USB firmware (for STM32MP13x lines
lines) │ │ │ ├── recipes-graphics │ │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ ├── recipes-kernel │ │ │ │ ├── linux Recipes for Linux kernel │ │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ ├── recipes-security │ │ │ │ └── optee Recipes for OPTEE │ │ │ ├── recipes-st │ │ │ │ └── images Recipes for the bootfs and userfs partitions binaries │ │ │ └── [...] │ │ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ │ └── scripts │ │ ├── envsetup.sh Environment setup script for Distribution Package │ │ └── [...] │ └── openembedded-core Core metadata for current versions of OpenEmbedded (standard)