STM32MP15 internal peripherals assignment table template

Revision as of 15:56, 1 February 2022 by Registered User (Nathalie Sangouard moved page Internal peripherals assignment table template to STM32MP15 internal peripherals assignment table template without leaving a redirect: GBA : STM32MP13 introduction )
Renaming.png This page is a candidate for renaming (move).
The requested new name is: STM32MP15 internal peripherals assignment table template .
The supplied reason is: STM32MP13 introduction .
-- Registered User (-) 16:11, 13 October 2021 (CEST).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.


STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)