X-LINUX-ACM Expansion Package

Revision as of 17:28, 1 July 2024 by Registered User (→‎Linux kernel)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)
Applicable for STM32MP25x lines

1. Article purpose[edit source]

X-LINUX-ACM is an OpenSTLinux distribution Expansion Package that targets the Acceleration Module feature in Linux® userland. The ACM platform is a switched endpoint for Ethernet-based industrial automation networks. It allows to improve the network performance by enabling a cut through forwarding mechanism next to standard conform Ethernet traffic. The ACM platform is a complete system architecture to allow fast frame processing (FFP) operations.

2. X-LINUX-ACM expansion package description[edit source]

2.1. Overview[edit source]

The X-LINUX-ACM is a package which provides a distribution package to generate a series of software to manage ACM.

2.2. Main software modification[edit source]

2.2.1. Linux kernel[edit source]

The X-LINUX-ACM need to have several kernel modules to enable the hardware for Time-Sensitive Networking (TSN):

  • st-stm32-deip glue module to enable specific hardware configuration for TSN
  • edge module to enable hardware TSN feature
  • acm module to enable ACM feature

2.2.2. User space additional stacks[edit source]

The X-LINUX-ACM provides a series of userland tools and component for Time-Sensitive Networking (TSN).

2.3. Main restrictions[edit source]

The X-LINUX-ACM is targeted to be demonstrate on the following target:

  • STM32MP257F-EV1 More info green.png

2.4. Versioning[edit source]

The latest version of X-LINUX-ACM Expansion Package is 5.1.0.
The X-LINUX-ACM Expansion Package is based to be used with OpenSTLinux distribution ecosystem release v5.1.0 More info.png .

2.5. Associated licenses[edit source]

See X-LINUX-ACM licenses.

3. Prerequisites[edit source]

3.1. Hardware prerequisites[edit source]

STM32MP257F-EV1.jpg

STM32MP257x-EV1 - hardware description

3.2. Software prerequisites[edit source]

The X-LINUX-ACM Expansion Package runs with OpenSTLinux ecosystem release v5.1.0 More info.png .

4. Hardware setup[edit source]

STM32MP257x-EV1 Evaluation board front side
STM32MP257F-EV1 shown here (picture is not contractual)


The Time-Sensitive Networking (TSN) is available only via the two ethernet port indicated 31 and 32.

5. Software setup[edit source]

5.1. How to install distribution package[edit source]

With the following procedure, the complete distribution is regenerated by enabling the X-LINUX-ACM Expansion Package.

5.1.1. Download the STM32MPU Distribution Package[edit source]

For ecosystem release v5.1.0 More info.png :
Install the STM32MPU Distribution Package.

5.1.2. Install the X-LINUX-TSN environment[edit source]

  • Clone the meta-st-stm32mp-tsn-swch git repositories
cd <Distribution Package installation directory>/layers/meta-st
git clone -b mickledore https://github.com/STMicroelectronics/meta-st-stm32mp-tsn-swch.git
cd ../..
  • Source the build environment with the correct board and layer.

For STM32MP25x lines More info.png:

DISTRO=openstlinux-weston MACHINE=stm32mp2 source layers/meta-st/scripts/envsetup.sh
bitbake-layers add-layer ../layers/meta-st/meta-st-stm32mp-tsn-swch

5.1.3. Build the image[edit source]

bitbake st-image-weston
Info white.png Information
Note that building the image might take a long time depending on the host computer performance.

5.2. How to populate the flash memory with the image[edit source]

Follow this link to see how to program the built image.

6. References[edit source]