1. Article purpose[edit source]
The article aims to help rebase an STM32 MPU project on a new ecosystem release by focusing on the impacts of the main changes.
2. Scope of this article[edit source]
This article provides some details for the main changes between STM32 MPU ecosystem release v5.0.0 and new STM32 MPU ecosystem release v5.1.0 . The aim is to help migrate your project.
All Information about the features delivered in the new release is also available in the OpenSTLinux release note.
3. Impacted domains[edit source]
3.1. Yocto build environment for Distribution Package[edit source]
- None
3.2. Hardware configuration[edit source]
Check the device tree files for the STMP32 MPU board:
Linux® kernel: between Linux kernel v6.1-stm32mp-r2 (v6.1.82) and previous Linux kernel v6.1-stm32mp-r1 (v6.1.28)
- IIO consumer binding and channels configuration update. Links and examples updated in ADC device tree configuration example
U-Boot: between U-Boot v2022.10-stm32mp-r2 and previous U-Boot v2022.10-stm32mp-r1
- None
OP-TEE: between OP-TEE 3.19.0-stm32mp-r2 and previous OP-TEE 3.19.0-stm32mp-r1
- None
TF-A: between TF-A v2.8-stm32mp-r2 and previous TF-A v2.8-stm32mp-r1
- Chain of Trust (COT) binding update. Links updated in TF-A_BL2_Chain of trust implementation
3.3. System configuration[edit source]
- FIP only has been supported since the STM32 MPU ecosystem release v5.0.0 . NoFIP is no more supported.
3.4. Boot stages[edit source]
- None
3.5. Security[edit source]
- New ST_OPTEE_PROFILE is set on Yocto MACHINE to select OP-TEE configuration:
3.6. User space and applications[edit source]
- None
4. References[edit source]