This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Warning_white.png (64 × 64 pixels, file size: 1 KB, MIME type: image/png)
File history
Click on a date/time to view the file as it appeared at that time.
Date/Time | Thumbnail | Dimensions | User | Comment | |
---|---|---|---|---|---|
current | 13:38, 8 October 2021 | ![]() | 64 × 64 (1 KB) | Registered User | Merge articles upload |
You cannot overwrite this file.
File usage
More than 100 pages use this file. The following list shows the first 100 pages that use this file only. A full list is available.
- ADC device tree configuration
- BKPSRAM internal memory
- Blktrace
- Core dump
- Cross-compile with OpenSTLinux SDK
- DMAMUX device tree configuration
- DMA device tree configuration
- Development setup for STM32MPU Embedded Software
- Dmesg and Linux kernel log
- Ethtool
- Example of directory structure for Packages
- FMC device tree configuration
- Ftrace
- GDB
- GPIO device tree configuration
- Gdbgui
- Gst-discoverer
- Gst-play
- Gst-typefind
- How to configure TF-A BL2
- How to create your own image
- How to create your own machine
- How to cross-compile with the Developer Package
- How to debug TF-A BL2
- How to launch Khronos OpenGLES conformance tests
- How to launch glmark2 benchmark
- How to setup a WLAN connection
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- I2C device tree configuration
- I2C i2c-tools
- IP Linux command line
- Ifconfig
- Kmemleak
- LPTIM device tree configuration
- LTTng
- Linux remoteproc framework overview
- Linux tracing, monitoring and debugging
- Ltrace
- MDMA device tree configuration
- Netdata
- Netstat
- OTG device tree configuration
- OpenEmbedded - devtool
- PC prerequisites
- PC prerequisites about STM32MPU distribution for Android
- Perf
- Pinctrl device tree configuration
- QUADSPI device tree configuration
- SAI device tree configuration
- SDMMC device tree configuration
- SPDIFRX Linux driver
- STM32CubeProgrammer
- STM32CubeProgrammer flashlayout
- STM32MP157x-DKx - board assembly
- STM32MP157x-DKx - board connections
- STM32MP157x-DKx - hardware description
- STM32MP157x-EV1 - board assembly
- STM32MP157x-EV1 - board connections
- STM32MP157x-EV1 - hardware description
- STM32MP15 Discovery kits - Starter Package
- STM32MP15 Discovery kits - required material
- STM32MP15 Discovery kits - starting for the first time
- STM32MP15 Evaluation boards - Starter Package
- STM32MP15 Evaluation boards - required material
- STM32MP15 Evaluation boards - starting for the first time
- STM32MP15 U-Boot
- STM32MP15 V4L2 camera overview
- STM32MP1 Developer Package
- STM32MP1 Developer Package - SDK
- STM32MP1 Developer Package - STM32CubeMP1 Package
- STM32MP1 Distribution Package
- STM32MP1 Distribution Package - OpenSTLinux distribution
- STM32MP1 Starter Package - images
- STM32 MPU Flash mapping
- STM32 MPU OpenSTLinux release note
- STM32 MPU ecosystem release note
- Serial TTY device tree configuration
- Soundcard configuration
- Strace
- Subpart - STM32MP1 - Starter Package
- Sysprof
- Sysstat tool suite
- TIM device tree configuration
- Tcpdump
- Trace-cmd and kernelshark trace viewer
- Trace and debug tools assignment table template
- U-Boot overview
- USBH device tree configuration
- Valgrind
- Wayland Weston overview
- Yavta
- Template:Board$
- Template:Green
- Template:Grey
- Template:PC$
- Template:Warning
- Category:Android
- Category:STM32MPU Embedded Software distribution for Android
- WikiAdmin:Wiki instance maintenance
View more links to this file.