This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains how to assemble the STM32MP157x-DKx Discovery kits. It is valid for the STM32MP157A-DK1, STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
The STM32MP157x-DKx Discovery kits packages (STM32MP157A-DK1, STM32MP157C-DK2 and STM32MP157F-DK2) are delivered assembled, and contain the items listed below. A USB Type-C™ cable is also included.
Please note that;
- the STM32MP157A-DK1 Discovery kit neither includes the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
- the STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kits include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
Position | Description |
---|---|
1 | MB1272 motherboard ("WLAN + Bluetooth" component included only for the STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kits) |
2 | MB1407 daughterboard DSI display (480x800 pixels): only for the STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kits |
3 | microSD card |