STM32 Sniffer for BLE User guide

Revision as of 08:52, 19 July 2023 by Registered User (→‎Following a connection)

This article provides information about how to use the STM32 sniffer for Bluetooth® Low Energy with Wireshark. For this tutorial, we presume that you have already installed the sniffer, but if this is not the case, you can follow this guide.

1. Starting the capture

Plug in your sniffer board and open Wireshark.

1.1. Optional configuration

  • In Wireshark, click on the wheel on the left side of the STM32 sniffer interface to open the interface configuration menu.
  • The channel index parameter is the channel on which the sniffer will listen when started. It can be changed on the fly later on. The default channel index is 39.
  • This is the channel index, not the frequency index (the primary advertising channel indexes are 37, 38, and 39).
Channel index
Connectivity Sniffer Optional Parameters.png


1.2. Launching the capture

To start the capture:

puce1.png
Click once to select the interface.
puce2.png
Click on start capturing.

or

puce1.png
Double click on the interface.
Starting the capture
Connectivity Sniffer Start Capture.png


1.3. Sniffer started

You should now see the advertising packets on the channel you configured.

puce1.png
On startup, the default target BD address is set to 00:00:00:00:00:00, meaning that no target is set, so packets from all devices are displayed.
Target BD address
Connectivity Sniffer Started.png


2. Following a connection

When the sniffer is running, it reports advertising and scan requests of all devices. You can then set the BD address of the target device that you want to follow when a connection to it occurs.

puce1.png
Set the target BD address.
puce2.png
Apply changes.
Setting a target to follow
Connectivity Sniffer Target1.png
Connectivity Sniffer Target2.png


Now you should only see:

  • Advertising and scan response packets from the target.
  • Scan requests to the target.
  • Connection packets from and to the target.
Target set
Connectivity Sniffer Target3.png


If after setting the target there are no more incoming packets, either:

  • There is no device with this BD address advertising on this channel.
  • The sniffer has not received the command; set the target again. (You will need to make a change to be able to apply changes; just delete the last number and re-enter it.)

Now if a device connects to your target and the sniffer intercepts the CONNECT_IND packet, you will start to see the communications between the two devices.

Info white.png Information
The sniffer only listens on one advertising channel, so it may not intercept a connection request on the first try if it was made on another channel. In this case, reconnect to your target. You can also use the multiple interfaces capture to improve the connection request interception success rate.



Connection intercepted
Connectivity Sniffer Connected1.png


The screen as shown above contains some additional data, where:

  • The direction column indicates the direction of the packets.
  • The color of the lines alternates with each connection event.

If the connection is terminated or if the sniffer loses it, it will return to the advertising channel you configured before.

3. Multiple interfaces capture

Because the sniffer can listen to only one channel at a time, capturing from multiple hardware interfaces can be very useful. You can capture traffic and pick up connect requests on all channels. You can also follow multiple links.

To capture with multiple sniffers, plug in your boards and:

puce1.png
Use CTRL or SHIFT and click to select the interfaces you want.
puce2.png
Click on start capturing.
Start capturing from multiple interfaces
Connectivity Sniffer Start Multiple Captures.png


During the capture, you can identify on which sniffer the packets have been captured:

puce1.png
In the Interface column, you can see the interface number corresponding to the com port number.
puce2.png
In the STMicroelectronics BLE sniffer dissection tree, you can see the Board ID field corresponding to the com port number.
Capture example from multiples interfaces

Connectivity Sniffer Multiple Capture Column.png

Connectivity Sniffer Multiple Capture ID.png


Warning white.png Warning
With multiple interfaces, the timestamp and timestamp difference are not relevant, because the boards have no synchronized timestamps.

To control each sniffer:

puce1.png
Click on the interface dropdown list and choose the one you want to control, as shown in the figure below.
Controlling multiples interfaces

Connectivity Sniffer Multiple Capture Toolbar.png


If you want each sniffer to be able to intercept a different channel, set a different target BD address for each sniffer.

4. Key input


For links that will be encrypted without debug mode or legacy pairing just work, the sniffer needs additional data to decrypt the traffic. On the right side of the toolbar, there is a key type selector with an associated value field. This input gives you the possibility to provide additional data that the sniffer can't know just by listening to the over-the-air communications.

You can enter the following data:

  • Legacy passkey: the key entered shall be 128 bits wide. The PassKey shall be zero-padded. For example, if the passkey were 401190 (decimal) -> 0x61F26 (hexadecimal), you shall enter: 000000000000000000000000000061F6.
  • Legacy OOB data: the key entered shall be 128 bits wide. The value shall be entered with the MSO on the leftmost byte.
  • LTK: the key entered shall be 128 bits wide. The value shall be entered with the MSO on the leftmost byte. The key will be used during a secure connection pairing if none of the devices are in debug mode.

The key shall be entered:

  • The pairing start for the legacy PassKey and OOB data.
  • Before the LL encryption start for the LTK.

If you encounter any problems, read the Troubleshooting article.

No categories assignedEdit