This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Track the most recent changes to the wiki on this page.
List of abbreviations:
- N
- This edit created a new page (also see list of new pages)
- m
- This is a minor edit
- b
- This edit was performed by a bot
- (±123)
- The page size changed by this number of bytes
21 November 2024
N 18:18 | Connectivity:Bluetooth qualification workspace example with STM32WB55 diffhist +6,692 Registered User (Creation of step by step example with qualification process and STM32WB55) |
N 10:17 | ISP:ISP introduction diffhist +2,037 Registered User (Created page with "<div class="res-img"> center| 250px |link= </div> An image signal processor ('''ISP''') converts RAW image captured by a RAW sensor into a digital image. It is done by adjusting the ISP image quality parameters such as brightness, contrast, and color balance.<br>The STM32 '''DCMIPP''' (Digital Camera Interface Pixel Pipeline), an internal peripheral which is the pixel pipeline section of a camera subsystem, embeds an ISP developped by STMicroelect...") |
20 November 2024
11:00 | STM32 KeygenTool diffhist −24 Registered User (Changed categories.) |
N 10:51 | Security:STM32N6 ROM trace analyzer diffhist +749 Registered User (Created page with "== ROM trace analysis procedure == ROM code traces cannot be downloaded directly. The process to get traces consists to use a special FSBL that will print the traces on UART. Here is a link where to download the FSBL sources : Load_a_signed_FSBL_and_get_the_BootRom_traces By default this FSBL permits to display bootrom traces on UART @115200 bauds, 8bits, 1 stop bit,...") |
00:51 | Category:Getting Started wtih STM32 Command Line tools diffhist +26 Registered User (→test: new section) |
18 November 2024
N 05:29 | Category:Getting Started wtih STM32 Command Line tools diffhist +1 Registered User (saving page) |
16 November 2024
N 20:55 | Category:ISP - Tools diffhist +57 Registered User (Created page with "{{:ISP Tools}} <noinclude> Category:ISP </noinclude>") |
N 20:50 | Category:ISP - How to diffhist +67 Registered User (Created page with "{{:ISP How to articles}} <noinclude> Category:ISP </noinclude>") |
N 20:48 | Category:ISP - Application examples diffhist +71 Registered User (First draft) |
15 November 2024
N 17:11 | ISP:Simple ISP preview diffhist +240 Registered User (First draft) |
N 17:02 | Connectivity:STM32WB0 BLE security diffhist +21,137 Registered User (Created page with "{{DISPLAYTITLE:STM32WB0 Bluetooth<sup>®</sup> LE Security}} ==Bluetooth<sup>®</sup> Low Energy security overview== This article provides a basic understanding of Bluetooth<sup>®</sup> Low Energy security features. It explains the different security features, how to setup these features on STM32WB, STM32WB0 and STM32WBA, how to decrypt the traffic using a sniffer and additional information regarding Bluetooth<sup>®</sup> Low Energy characteristics and security permis...") |
16:59 | Connectivity:STM32WB0 BLE Privacy diffhist +29 Registered User (Changed categories.) |
N 15:26 | Connectivity:Wifi X-CUBE-WW6 Architecture Overview (2) diffhist +19,633 Registered User (Created page with "{{ArticleToRename | X-CUBE-ST67W61 Architecture | Renamed project due to RFOC migration}} {{DISPLAYTITLE:X-CUBE-ST67W61 Architecture}} back to main page {{UnderConstruction}} Please understand this is draft, thank you == General description == === Introduction === X-CUBE-ST67W61 is a set of software components implementing Host applications driving a Wi-Fi and BLE coprocessor (ST67W611M). The co-processor is controlled via AT co...") |