This page lists tracking categories which are automatically populated by the MediaWiki software. Their names can be changed by altering the relevant system messages in the MediaWiki namespace.
Tracking category | Message name | Category inclusion criteria |
---|---|---|
Pages with broken file links (1 C, 4 P) | broken-file-category | The page contains a broken file link (a link to embed a file when the file does not exist). |
Pages using duplicate arguments in template calls (empty) | duplicate-args-category | The page contains template calls that use duplicates of arguments, such as {{foo|bar=1|bar=2}} or {{foo|bar|1=baz}} . |
Pages where expansion depth is exceeded (empty) | expansion-depth-exceeded-category | The page exceeds the maximum expansion depth. |
Pages with too many expensive parser function calls (empty) | expensive-parserfunction-category | The page uses too many expensive parser functions (like #ifexist ). See Manual:$wgExpensiveParserFunctionLimit. |
Hidden categories (empty) | hidden-category-category | The category contains __HIDDENCAT__ in its page content, which prevents it from showing up in the category links box on pages by default. |
Indexed pages (empty) | index-category | The page has a __INDEX__ on it (and is in a namespace where that flag is allowed), and hence is indexed by robots where it normally wouldn't be. |
Pages where node count is exceeded (empty) | node-count-exceeded-category | The page exceeds the maximum node count. |
Noindexed pages (1 C, 2 P, 1 F) | noindex-category | The page is not indexed by robots because it has the magic word __NOINDEX__ on it and is in a namespace where that flag is allowed. |
Pages with non-numeric formatnum arguments (empty) | nonnumeric-formatnum | The page contains a non-numeric argument to the formatnum parser function. |
Pages containing omitted template arguments (empty) | post-expand-template-argument-category | The page is bigger than $wgMaxArticleSize after expanding a template argument (something in triple braces, like {{{Foo}}} ). |
Pages where template include size is exceeded (empty) | post-expand-template-inclusion-category | The page size is bigger than $wgMaxArticleSize after expanding all the templates, so some templates were not expanded. |
Pages with ignored display titles (empty) | restricted-displaytitle-ignored | The page has an ignored {{DISPLAYTITLE}} because it is not equivalent to the page's actual title. |
Pages which use = as a template (empty) | template-equals-category | The page contains {{=}} but on this wiki that does not expand to = . This usage is deprecated; a future MediaWiki version will implement {{=}} as a parser function. |
Pages with template loops (empty) | template-loop-category | The page contains a template loop, ie. a template which calls itself recursively. |
Pages where the unstrip depth limit is exceeded (empty) | unstrip-depth-category | The page exceeds the unstrip depth limit. |
Pages where the unstrip size limit is exceeded (empty) | unstrip-size-category | The page exceeds the unstrip size limit. |
Category is disabled | dpl-tag-tracking-category | No description available. |
Pages using DynamicPageList3 Intersection parser tag (empty) | dpl-intersection-tracking-category | No description available. |
Category is disabled | dpl-parserfunc-tracking-category | No description available. |
Pages using DynamicPageList3 dplnum parser function (empty) | dplnum-parserfunc-tracking-category | No description available. |
Pages using DynamicPageList3 dplvar parser function (empty) | dplvar-parserfunc-tracking-category | No description available. |
Pages using DynamicPageList3 dplreplace parser function (empty) | dplreplace-parserfunc-tracking-category | No description available. |
Pages using DynamicPageList3 dplchapter parser function (empty) | dplchapter-parserfunc-tracking-category | No description available. |
Pages using DynamicPageList3 dplmatrix parser function (empty) | dplmatrix-parserfunc-tracking-category | No description available. |
Pages with RSS feeds (empty) | rss-tracking-category | The page has an RSS feed. |
Pages with script errors (empty) | scribunto-common-error-category | There was an error when processing the modules included on the page. |
Scribunto modules with errors (empty) | scribunto-module-with-errors-category | The module has an error in it. |
Pages with a PDF tag that were last edited by a user without permission to use the tag. (empty) | pdfembed-permission-problem-category | The page contains a <pdf> tag. |
Pages using Tabber parser tag (empty) | tabberneue-tabber-category | No description available. |
Pages using TabberTransclude parser tag (empty) | tabberneue-tabbertransclude-category | No description available. |
Pages with reference errors (empty) | cite-tracking-category-cite-error | Pages in this category have errors in the usage of references tags. |
Pages with syntax highlighting errors (empty) | syntaxhighlight-error-category | There was an error when attempting to highlight code included on the page. |
Pages using deprecated enclose attributes (empty) | syntaxhighlight-enclose-category | The syntaxhighlighting on the page uses deprecated enclose syntax. |
Pages using deprecated source tags (empty) | syntaxhighlight-source-category | The syntaxhighlighting on the page uses deprecated source tags. |
TemplateStyles stylesheets with errors (empty) | templatestyles-stylesheet-error-category | The TemplateStyles stylesheet has an error. |
Pages with TemplateStyles errors (empty) | templatestyles-page-error-category | There was an error when processing a <templatestyles/> tag on the page. |
Pages with math errors (empty) | math-tracking-category-error | Pages in this category have errors in the usage of math tags. |
Pages with math render errors (empty) | math-tracking-category-render-error | Pages in this category have rendering errors in the math tags. |
Pages that use a deprecated format of the chem tags (empty) | math-tracking-category-mhchem-deprecation | Pages in this category use a deprecated format of the chem tags |
Pages that use a deprecated format of the math tags (empty) | math-tracking-category-texvc-deprecation | Pages in this category use a deprecated format of the math tags |
Pages with graphs (empty) | graph-tracking-category | The page includes a <graph> tag. |
Pages with obsolete Vega 1.0 graphs (empty) | graph-obsolete-category | The page includes a <graph> tag that should be updated to version 2. |
Pages with broken graphs (empty) | graph-broken-category | The page includes a <graph> tag with invalid usage. |