This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Page title matches
- 398 bytes (48 words) - 08:00, 13 October 2021
- 3 KB (358 words) - 08:00, 13 October 2021
- 1 KB (162 words) - 16:04, 12 October 2021
- 178 bytes (21 words) - 08:40, 19 April 2024
- 1 KB (207 words) - 12:59, 25 April 2024
Page text matches
- === Perform ping test === To test the Ethernet connection, it is useful to know how to perform ...1 KB (162 words) - 16:04, 12 October 2021
- ===Running test suite=== Execute the following commands on the target board: ... [ 1] EGL: enable default configs for conformance test ...3 KB (358 words) - 08:00, 13 October 2021
- Use one of the following commands to quickly test the panel backlight: ... # switch on/off test (while true; do echo 0 > $bl; sleep 0.5; echo ...2 KB (223 words) - 08:02, 8 April 2022
- test for edition -- Nathalie Sangouard (talk) 10:40, 19 April 2024 (CEST)add comment review ...178 bytes (21 words) - 08:40, 19 April 2024
- rngtest is a basic test that checks data using FIPS 140-2 tests ... which is a security requirement test for cryptographic module compliance. ...3 KB (355 words) - 15:57, 12 October 2021
- (See the How to test core dump service below ). ==How to test core dump== * Launch a program Launch a program (for ...4 KB (514 words) - 09:44, 24 October 2022
- firmware package for DDR configuration and test on device=1 ... UTIL firmware package for DDR configuration and test on ...2 KB (268 words) - 16:08, 29 June 2023
- in microSDTM card and is used to load the test application from microSD™ ... :This binary is the test application, programmed in microSD™ card ...7 KB (1,095 words) - 10:46, 21 November 2023
- stm32 in eMMC™ and is used to load the test application from eMMC™ to DDR. ... :This binary is the test application, programmed in eMMC™ via STM32PRGFW_ ...9 KB (1,276 words) - 09:13, 15 March 2024
- speaker-test -D playback_spdif -c 2 -F S32_LE -f 440 -t sine -l 1 ... speaker-test -c 2 -F S32_LE -f 440 -t sine -l 1 10391 | 2019-01-21 ...4 KB (629 words) - 11:46, 8 June 2022