{

   "filename": "Setup.gdb.txt",
   "filetimestamp": "20190425131945",
   "namespace": 6,
   "titletext": "Setup.gdb.txt",
   "action": "edit",
   "summary": "Add command \"set arm abi AAPCS\".\nWhen gdb loads an ELF file to the target, it will get the \"abi\" from the file header.  But on most of MPU use cases the binary is already in the target's memory so the \"abi\" has to be set explicitly.\nWithout the correct \"abi\" set, gdb will try to guess the stack frame reading in memory at the addresses in registers r7 and r11, which are not always valid addresses.",
   "parentid": 0,
   "id": 1836,
   "ownerid": 128,
   "type": "filesave",
   "archived": false,
   "tags": [],
   "resolved": false

}

No categories assignedEdit