Last edited 3 weeks ago

Latest wiki

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This page aims to provide link to the flagship/latest wiki. Each STM32 MPU ecosystem release flow has its corresponding wiki.

An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the below table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.

The most recent flow is associated with the flagship/latest wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

This current wiki is the wiki for the v6 flow (v6.y.z ecosystem releases): if you need information about this ecosystem releases flow, continue browsing this wiki.

However, if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to browse the flagship/latest wiki that contains the latest major ecosystem release:

STM32 MPU wiki by ST.png
STM32 MPU flagship/latest wiki for the v6.y.z ecosystem releases
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
STM32 MPU flagship/latest wiki for v6 flow

(for STM32 Arm® Cortex® MPUs More info.png)

v6.2.0 (Feb 2026) (for STM32MP1 series and STM32MP2 series)
v6.1.0 (Jun 2025) (for STM32MP1 series, STM32MP23x lines More info.png and STM32MP25x lines More info.png)
v6.0.0 (Nov 2024) (for STM32MP1 series and STM32MP25x lines More info.png)

Linux® kernel v6.6 (LTS)
U-Boot v2023.10
TF-A v2.10
OP-TEE v4.0.0
OpenEmbedded v5.0 (Scarthgap)

Wiki for v5 flow

v5.1.0 (Jun 2024) (for STM32MP1 series and STM32MP25x lines More info.png)
v5.0.0 (Dec 2023) (for STM32MP1 series only)

Linux® kernel v6.1 (LTS)
U-Boot v2022.10
TF-A v2.8
OP-TEE v3.19.0
OpenEmbedded v4.2 (Mickledore)