Last edited 2 months ago

Wiki archives


This page aims to provide links to archived wikis.
Each STM32 MPU ecosystem release flow has its corresponding wiki.

An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.

The most recent flow is associated with the latest wiki also known as flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

The flagship wiki is for the v5 flow (v5.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to continue browsing the wiki that contains the latest major ecosystem release for STM32MP1 series.


However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:

Wikis and software components
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
This wiki - Wiki for v5 flow

(for STM32MP1 series)

v5.0.0

Linux® kernel v6.1 (LTS)
U-Boot v2022.10
TF-A v2.8
OP-TEE v3.19.0
OpenEmbedded v4.2 (Mickledore)

Archived wiki for the v4 flow

(for STM32MP1 series)

v4.1.0 (Nov 2022)
v4.0.0 (June 2022)

Linux® kernel v5.15 (LTS)
U-Boot v2021.10
TF-A v2.6
OP-TEE v3.16.0
OpenEmbedded v4.0 (Kirkstone)

Archived wiki for the v3 flow

(for STM32MP15x lines More info.png only)

v3.1.0 (Nov 2021)
v3.0.0 (Apr 2021)

Linux® kernel v5.10 (LTS)
U-Boot v2020.10
TF-A v2.4
OP-TEE v3.12.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v2 flow

(for STM32MP15x lines More info.png only)

Those releases are now deprecated
v2.1.0
v2.0.0

Linux® kernel v5.4 (LTS)
U-Boot v2020.01
TF-A v2.2
OP-TEE v3.9.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v1 flow

(for STM32MP15x lines More info.png only)

Those releases are now deprecated
v1.2.0
v1.1.0
v1.0.0

Linux® kernel v4.19 (LTS)
U-Boot v2018.11
TF-A v2.0
OP-TEE v3.3.0
OpenEmbedded v2.6 (Thud)