This article aims to present how to assemble the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 Evaluation board: the part numbers are specified in the STM32MP25 microprocessor part numbers article.
The STM32MP257x-EV1 Evaluation boards packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include all the items listed below.

Position | Description |
---|---|
1 | MB1936 main board |
2 | 7” LVDS WSVGA display with touch panel (EDT ETML0700Z9NDHA panel) |
3 | LVDS display FPC |
4 | MB1854 daughterboard AI camera (provided via B-CAMS-IMX package, not part of STM32MP257x-EV1 Evaluation boards packages) |
5 | camera board FFC (provided via B-CAMS-IMX package, not part of STM32MP257x-EV1 Evaluation boards packages) |
1. How to connect MB1854 camera board to MB1936[edit | edit source]
File:STM32MP257x-EV1 CameraBoardAssembly1.png
Camera board assembly (picture is not contractual)
- Find the camera port on STM32MP257x-EV1 Evaluation board (CN4) and the one on MB1854 (CN1). One FFC is provided in the camera box.
- On each port, carefully:
- lightly pull the black plastic (1) to insert the contact side of the FPC towards the board (2).
- Push the black plastic to hold the FFC (3).
File:STM32MP257x-EV1 CameraBoardAssembly2.png
Camera board assembly (picture is not contractual)
2. How to connect LVDS display to MB1936[edit | edit source]
File:STM32MP257x-EV1 DispalyBoardAssembly1.png
Display board assembly (picture is not contractual)
- Check the above cable orientation thanks to the black mark and the white twisted pairs.
- Find the LVDS port on STM32MP257x-EV1 Evaluation board (CN2) and the one on the display (CN1). One FPC is provided in the STM32MP257x-EV1 Evaluation board box.
- On each port, insert the cable as described:
File:STM32MP257x-EV1 DispalyBoardAssembly2.png
Display board assembly (picture is not contractual)
3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]