Revision as of 00:28, 27 January 2021 by Registered User

1. Create a "user space" project[edit source]

In context of Cortex-A7 sub-project, MP157C-DK2_CA7 here, right click and select Create a userspace Project..

User space project wizard shortcut

We select here Executable project type, in C language.

User space project creation wizard


2. Build[edit source]

  • Select your project, right-click and then Build Project.
Executable Build


3. Preparing Debug Configuration[edit source]

Your target must be Linux booted and network connected. Please, start Target Status widget on the bottom right and check for the green light.

Target Status - green


4. Debug Configuration[edit source]

  • Select your project, right-click Debug as... > Debug Configurations.
  • Then create a C/C++ Remote Application debug configuration, double clicking on it.

4.1. Main tab[edit source]

  • Fill a destination directory, for example: /tmp/UserSpaceExe
  • Select a connection: MPU SSH 
File:CubeIDE-UserSpace-Debug3.png
Debug configuration - main

4.2. Debugger tab[edit source]

Now set-up GDB Client with SDK one

  • For SDK embedded and installed inside STM32CubeIDE (e.g. with STM32CubeIDE v1.4.2) :<Stm32CubeIDEInstallDir>/plugins/com.st.openstlinux.sdk.openstlinux_5.4_dunfell_mp1_20_06_24_5.4.0.202007020712/tools/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-gdb
  • For SDK installed on disk : <SdkInstallDir>/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-gdb
File:CubeIDE-UserSpace-Debug4.png
Debug configuration - debugger


5. Debug[edit source]

Click Debug :

  1. Executable is downloaded to the target,
  2. GDBServer is launched on the target,
  3. GDBClient is launched on the workstation and can exchange via network with GDBServer,
Info white.png Information
in case of error; please check if GDBServer is still running on the target.