STM32MP257x-EV1 - board assembly

Revision as of 11:53, 11 December 2023 by Registered User
Applicable for STM32MP25x lines


This article aims to present how to assemble the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 More info green.png Evaluation board: the part numbers are specified in the STM32MP25 microprocessor part numbers article.

Warning white.png Warning
To start efficiently the board, it's recommended to go through its Starter Package article: Category:Starter Package


The STM32MP257x-EV1 Evaluation boards packages (STM32MP257F-EV1 More info green.png) include all the items listed below.

Out of the STM32MP257x-EV1 box STM32MP257F-EV1 shown here (picture is not contractual)
Position Description
1 MB1936 main board
2 7” LVDS WSVGA Color Display with touch panel
3 LVDS display connector
4 MB1854 daughterboard AI camera (provided via B-CAMS-IMX package)
5 Camera board connector (provided via B-CAMS-IMX package)


STM32MP257x-EV1 Evaluation board assembly
STM32MP257F-EV1 shown here (picture is not contractual)

1. How to connect MB1854 camera board to MB1936[edit source]

File:STM32MP257x-EV1 CameraBoardAssembly1.png

  • Find the Camera port on EV (CN4) and the one on MB1854 (CN1). One FPC is provided in the Camera box.
  • On each port, carefully:
    • lightly pull the black plastic (1) to insert the contact side of the FPC towards the board (2).
    • Push the black plastic to hold the FPC (3).

(picture is not contractual) File:STM32MP257x-EV1 CameraBoardAssembly2.png

2. How to connect LVDS display to MB1936[edit source]

File:STM32MP257x-EV1 DispalyBoardAssembly1.png

  • Check the above cable orientation thanks to the black mark and the white twisted pairs.
  • Find the LVDS port on EV (CN2) and the one on the display (CN1). One FPC is provided in the EV box.
  • On each port, insert the cable as described:

File:STM32MP257x-EV1 DispalyBoardAssembly2.png

3. STM32MP257x-EV1 Evaluation board assembled[edit source]


STM32MP257x-EV1 Evaluation board assembled
STM32MP257F-EV1 shown here (picture is not contractual)