Changes notification - v5.0.0

Revision as of 10:35, 6 July 2023 by Registered User (→‎Impacted domains)
Applicable for STM32MP13x lines, STM32MP15x lines


BackToNavigationTree button.png


1. Article purpose[edit source]

The article aims to help rebase an STM32 MPU project on a new ecosystem release by focusing on the impacts of the main changes.

2. Scope of this article[edit source]

This article provides some details for the main changes between STM32 MPU ecosystem release v4.1.0 and new STM32 MPU ecosystem release v5.0.0 More info.png . The aim is to help migrate your project.

All Information about the features delivered in the new release is also available in the OpenSTLinux release note.

Warning DB.png Important

In case of upgrade from OpenSTLinux ecosystem release v4.0.0, check first the previous release change notification available on wiki dedicated to the v4.y.z ecosystem releases:

3. Impacted domains[edit source]

3.1. Yocto build environment for Distribution Package[edit source]

  • None

3.2. Hardware configuration[edit source]

Check the device tree files for the STMP32 MPU board:

Linux® kernel: between Linux kernel v6.1-stm32mp-r1 (v6.1.28) and previous Linux kernel v5.15-stm32mp-r2 (v5.15.67)

  • None

U-Boot: between U-Boot v2022.10-stm32mp-r1 and previous U-Boot v2021.10-stm32mp-r2

  • None except alignment with Linux® kernel device tree

OP-TEE: between OP-TEE 3.19.0-stm32mp-r1 and previous OP-TEE 3.16.0-stm32mp-r2

  • Alignment with Linux® kernel device tree
  • For STM32MP15x lines More info.png:
    • OP-TEE build in DDR (pager OFF) : Some services are now default disabled
Warning white.png Warning
In case OP-TEE is configured for running in SYSRAM for STM32MP15x lines More info.png (See How_to_configure_OP-TEE#STM32MP15x_lines, please note that DVFS (System frequency scaling) must be disabled.


TF-A: between TF-A v2.8-stm32mp-r1 and previous TF-A v2.6-stm32mp-r2

  • Alignment with Linux® kernel device tree
  • BL2 always runs at 650MHz (PLL1 configuration removed from DT)
  • Move compatible to secure RCC from SoC DT to board DT
  • Shared memory with OP-TEE removed
  • For STM32MP15x lines More info.png
    • RCC configuration updated to follow new bindings
Info white.png Information
This is possible with git diff command to get delta between two branches in the same repository.
Example with STLINUX GitHub repository and for all STM32MP1 device tree files:

git diff v5.15-stm32mp-r2 v6.1-stm32mp-r1 -- arch/arm/boot/dts/stm32mp1*

3.3. System configuration[edit source]

  • None

3.4. Boot stages[edit source]

  • This ecosystem release v5.0.0 More info.png no more supports the TF-A SP-MIN as secure monitor.
    OP-TEE is only the supported BL32 and you must migrate the STM32MP15x lines More info.png projects to use it
  • The MTD partitions are defined in U-Boot device tree and no more in U-Boot defconfig

3.5. Security[edit source]

  • New implementation of a secure watchdog
  • New device-tree RNG configuration
  • Use of watchdog framework
  • Fix IWDG early-interrupt

3.6. User space and applications[edit source]

  • None

4. References[edit source]