How to create Signed FIT image from Distribution package

Revision as of 11:38, 17 June 2022 by Registered User (→‎Article purpose)

1. Article purpose[edit source]

The purpose of this article is to explain how to create a signed fit image signed which contains kernel image and devicetree.

Warning white.png Warning
With the actual implementation on Yocto/Openembedded, the creation of signing fit image request to declare only one devicetree on the machine

2. Creating signature key[edit source]

Yocto/Openembeded can create a key for signing fit image.
If you would like to create you own key, follow the command to generate manually a new signing key.

  • To generate manually a new signing key:

Create directory which receive siging key (here uboot-sign-directory for the example)

mkdir uboot-sign-directory/

Generate RSA private key for signing fitImage

 openssl genrsa -F4 \
       -out  uboot-sign-directory/my-uboot-sign-key.key \
       2048

Generate certificate for signing fitImage

 openssl req -batch -new -x509 \
     -key uboot-sign-directory/my-uboot-sign-key.key \
     -out uboot-sign-directory/my-uboot-sign-key.crt

3. Configuration of Machine on Distribution Package[edit source]

On the Yocto/Openembedded machine you need to specify several parameter:

  • force to use fit image
  • request to sign the fit image
  • specify the path of signing key


3.1. Use fit image[edit source]

# to use fit image for kernel and devicetree
 MACHINE_FEATURES += "fit"

3.2. Use Signing FIT[edit source]

UBOOT_SIGN_ENABLE = "1"

3.3. Signing key[edit source]

if you key are localized on a specific directory like $HOME/uboot-sign-directory (put an asbolute path)

 UBOOT_SIGN_KEYDIR = "$HOME/uboot-sign-directory"

or if you would like to use a generic path

 UBOOT_SIGN_KEYDIR = "${DEPLOY_DIR_IMAGE}"

For Signing key, you MUST specify the name of the key (without the extension), my-uboot-sign-key for example

UBOOT_SIGN_KEYNAME = "my-uboot-sign-key"

If you would like that the Distribution Pakage generate the signing key, you need to add the following key in addition to UBOOT_SIGN_ENABLE

FIT_GENERATE_KEYS = "1"

3.4. Summary: Machine contents[edit source]

# to use fit image for kernel and devicetree
MACHINE_FEATURES += "fit"
#signing key
UBOOT_SIGN_KEYDIR = "${DEPLOY_DIR_IMAGE}"
UBOOT_SIGN_KEYNAME = "my-uboot-sign-key"
# Sign fit image
UBOOT_SIGN_ENABLE = "1"
# generate new signing key if not exist
FIT_GENERATE_KEYS = "1"
# Uboot mkimage option
UBOOT_MKIMAGE_DTCOPTS = "-I dts -O dtb -p 2000"


4. References[edit source]



No categories assignedEdit