Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
This article aims to give the following information:
- How to download and install the latest SDK for the STM32 microprocessor Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v1.1.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xz
- Download and install the STM32MP1 SDK.
- By downloading this software package, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v1.1.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xz
$ chmod +x stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh
$ ./stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.4-openstlinux-4.19-thud-mp1-19-10-09 ====================================================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? Y Extracting SDK.......................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /<working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note. |
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-openstlinux_weston_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
2. Archives[edit source]
2.1. STM32MP15-Ecosystem-v1.0.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz
- Download and install the STM32MP1 SDK.
- By downloading this software package, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v1.0.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz
$ chmod +x stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh
$ ./stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.4-openstlinux-4.19-thud-mp1-19-02-20 ====================================================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? Y Extracting SDK.......................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /<working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note. |
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-openstlinux_weston_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi