X-LINUX-QT Developer Package - SDK

Revision as of 18:08, 16 July 2024 by Registered User
Applicable for STM32MP25x lines


This article aims to give the following information:

  • How to download and install the latest X-LINUX-QT SDK-Addon for the STM32 microprocessor series.
  • Where to find the associated release note.
  • Where to find the previous releases (archives).
Warning white.png Warning
To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor series: Category:Developer Package

1. X-LINUX-QT SDK-Addon v1.0.0 release[edit source]

The X-LINUX-QT SDK-Addon is delivered through two tarball files named :

  • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz for x86_64 host architecture
  • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz for arm64 host architecture

Download and install the X-LINUX-QT SDK-Addon. The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

X-LINUX-QT Developer Package SDK-Addon v1.0.0 release
Download
  • Go on st.com to download
    • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz file for x86_64 host architecture
    • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz file for arm64 host architecture
Installation

For x86_64 host architecture

  • Uncompress the tarball file to get the SDK installation script.
 mkdir -p ~/MySDK
 tar xvf en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz -C ~/MySDK
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
 cd <working directory absolute path>/Developer-Package/SDK
 ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
  • A successful installation outputs the following log:
===============================================================================================================================================
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version unknown component - X-LINUX-QT version 1.0.0 SDK-Addon installer
===============================================================================================================================================
Extracting X-LINUX-QT-Addon SDK................................................................................................Done.
Setting it up... Done.


Using /home/bbkarim/Qt/Tools/sdktool/libexec/qtcreator/sdktool
Adding "Qt 5.15.13 for STM32MP25 ( 4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, X-LINUX-QT v1.0.0)" kit for Qt Creator... Done.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

For arm64 host architecture

  • Uncompress the tarball file to get the SDK installation script.
 mkdir -p ~/MySDK
 tar xvf en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz -C ~/MySDK
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
 cd <working directory absolute path>/Developer-Package/SDK
 ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk/{{X-
  • A successful installation outputs the following log:
==================================================================================================================================================
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26 - X-LINUX-QT version 1.0.0 SDK-Addon installer
===================================================================================================================================================
Extracting X-LINUX-QT-Addon SDK......................................................................................................... Done.
Setting it up... Done.
Using /home/bbkarim/Qt/Tools/sdktool/libexec/qtcreator/sdktool
Adding "Qt 5.15.13 for STM32MP25 ( 4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, X-LINUX-QT v1.0.0)" kit for Qt Creator... Done.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.
Release note



2. Archives Archive box.png[edit source]

N.A.