This article aims to present how to assemble the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 Evaluation board: the part numbers are specified in the STM32MP25 microprocessor part numbers article.
The STM32MP257x-EV1 Evaluation boards packages (STM32MP257F-EV1 ) include all the items listed below.
![Out of the STM32MP257x-EV1 box STM32MP257F-EV1 shown here (picture is not contractual) Out of the STM32MP257x-EV1 box STM32MP257F-EV1 shown here (picture is not contractual)](/stm32mpu/nsfr_img_auth.php/thumb/e/e2/STM32MP257x-EV1_split.jpg/800px-STM32MP257x-EV1_split.jpg)
Position | Description |
---|---|
1 | MB1936 main board |
2 | 7” LVDS WSVGA display with touch panel ( EDT ETML0700Z9NDHA panel) |
3 | LVDS display cable |
4 | MB1854 daughterboard AI camera (provided via B-CAMS-IMX package) |
5 | Camera board cable (provided via B-CAMS-IMX package) |
1. How to connect MB1854 camera board to MB1936[edit source]
File:STM32MP257x-EV1 CameraBoardAssembly1.png
- Find the Camera port on EV (CN4) and the one on MB1854 (CN1). One FPC is provided in the Camera box.
- On each port, carefully:
- lightly pull the black plastic (1) to insert the contact side of the FPC towards the board (2).
- Push the black plastic to hold the FPC (3).
(picture is not contractual) File:STM32MP257x-EV1 CameraBoardAssembly2.png
2. How to connect LVDS display to MB1936[edit source]
File:STM32MP257x-EV1 DispalyBoardAssembly1.png
- Check the above cable orientation thanks to the black mark and the white twisted pairs.
- Find the LVDS port on EV (CN2) and the one on the display (CN1). One FPC is provided in the EV box.
- On each port, insert the cable as described:
File:STM32MP257x-EV1 DispalyBoardAssembly2.png
3. STM32MP257x-EV1 Evaluation board assembled[edit source]