STM32MP257x-EV1 - board connections

Revision as of 13:15, 4 December 2023 by Registered User
Applicable for STM32MP25x lines


This article aims to present the recommended connections to start with the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 More info green.png Evaluation board : the part numbers are specified in the STM32MP25 microprocessor part numbers article.

Warning white.png Warning
To start efficiently the board, it's recommended to go through its Starter Package article: Category:Starter Package


STM32MP257x-EV1 connections.jpg



USB Power - STLINK TypeCETHERNET 2 / PHY ETH2ETHERNET 1 / PHY ETH1ETHERNET 3 / PHY ETH32 x USB type A (host) → E.g. mouse  Keyboard  USB driver...USB2.0 DRD TypeC  →  PC consoleMicroSD card slotDSI connectorGPIO Expansion connectorMini-PCIe connectorMB1936 5V/3A Power Supply JackFDCAN2FDCAN1
STM32MP257x-EV1 Evaluation board connections

STM32MP257F-EV1 shown here (picture is not contractual)


rect 4 1220 145 1376 USB micro-B (ST-LINK/V2-1) → PC virtual COM port and debug

Reset button