STM32MP2 Developer Package - SDK

Revision as of 14:04, 22 November 2023 by Registered User
Applicable for STM32MP25x lines

This article aims to give the following information:

  • How to download and install the latest SDK for the STM32 microprocessor series.
  • Where to find the associated release note.
  • Where to find the previous releases (archives).
Warning white.png Warning
To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor series: Category:Developer Package

1. STM32MPU-Ecosystem-v5.0.0.BETA release[edit source]

The STM32MP2 SDK is delivered through two tarball file named :

  • unknown revision for x86_64 host architecture
  • unknown revision for arm64 host architecture

Download and install the STM32MP2 SDK. The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP2 Developer Package SDK - STM32MP2-Ecosystem-v5.0.0.BETA release
Download
  • Go on st.com to download
    • unknown revision file for x86_64 host architecture
    • unknown revision file for arm64 host architecture
Installation For x86_64 host architecture
  • Uncompress the tarball file to get the SDK installation script.
 tar xvf unknown revision
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x unknown revision/unknown revision
  • Run the SDK installation script.
    • Use the -d <SDK installation directory absolute path> option to specify the absolute path to the directory in which you want to install the SDK (<SDK installation directory>).
    • If you follow the proposition to organize the working directory, it means:
 ./unknown revision/unknown revision -d <working directory absolute path>/Developer-Package/SDK
  • A successful installation outputs the following log:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
===================================================================================================================================
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? 
Extracting SDK.........................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa35-ostl-linux

For arm64 host architecture

 tar xvf unknown revision
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x unknown revision/unknown revision
  • Run the SDK installation script.
    • Use the -d <SDK installation directory absolute path> option to specify the absolute path to the directory in which you want to install the SDK (<SDK installation directory>).
    • If you follow the proposition to organize the working directory, it means:
 ./unknown revision/unknown revision -d <working directory absolute path>/Developer-Package/SDK
  • A successful installation outputs the following log:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
===================================================================================================================================
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? 
Extracting SDK.........................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa35-ostl-linux
Release note

Details about the content of the SDK are available in the associated STM32 MPU ecosystem release note.

Archive box.png If you are interested in older releases, please have a look into the section Archives.

  • The SDK is in the <SDK installation directory>:
<SDK installation directory>                                      SDK for OpenSTLinux distribution: details in Standard SDK directory structure article
├── environment-setup-cortexa35-ostl-linux                        Environment setup script for Developer Package
├── site-config-cortexa35-ostl-linux
├── sysroots
│   ├── cortexa35-ostl-linux                                      Target sysroot (libraries, headers, and symbols)
│   │   └── [...]
│   └── x86_64-ostl_sdk-linux                                     Native sysroot (libraries, headers, and symbols)
│       └── [...]
└── version-cortexa35-ostl-linux

For arm64 host architecture

<SDK installation directory>                                      SDK for OpenSTLinux distribution: details in Standard SDK directory structure article
├── environment-setup-cortexa35-ostl-linux                        Environment setup script for Developer Package
├── site-config-cortexa35-ostl-linux
├── sysroots
│   ├── cortexa35-ostl-linux                                      Target sysroot (libraries, headers, and symbols)
│   │   └── [...]
│   └── aarch64-ostl_sdk-linux                                     Native sysroot (libraries, headers, and symbols)
│       └── [...]
└── version-cortexa35-ostl-linux


2. Archives Archive box.png[edit source]

This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.