1. Open a terminal[edit source]
Open a terminal on the host computer.
![](/stm32mpu/nsfr_img_auth.php/9/99/Ubuntu_terminal.png)
Ubuntu terminal
All the commands preceded by have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace cd $HOME/STM32MPU_workspace
2. Check the host computer Internet access[edit source]
- An Internet access through http and https protocols must be provided.
The command below enables checking for Internet access through http/https protocols:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.
Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:
export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access using the command:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
3. Install the tools[edit source]
3.1. STM32CubeProgrammer[edit source]
- Create your STM32MPU tools directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
- Download STM32CubeProgrammer (via st.com), in the following directory : $HOME/STM32MPU_workspace/tmp
STM32CubeProgrammer v2.14.0 is recommended for ecosystem release v5.0.0.
- Uncompress the archive file to get the STM32CubeProgrammer installers:
cd $HOME/STM32MPU_workspace/tmp unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
./SetupSTM32CubeProgrammer-x.y.z.linux
The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples and are still valid for higher versions :
![](/stm32mpu/nsfr_img_auth.php/2/2d/STM32CubeProgrammer_installation_splashscreen.png)
Splash screen
![](/stm32mpu/nsfr_img_auth.php/d/d6/STM32CubeProgrammer_installation_welcome_27.png)
Welcome page
![](/stm32mpu/nsfr_img_auth.php/b/b5/STM32CubeProgrammer_installation_path_25.png)
Installation path
- Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h ------------------------------------------------------------------- STM32CubeProgrammer vx.y.z -------------------------------------------------------------------
3.2. USB serial link[edit source]
- Install the libusb on your host computer:
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules sudo cp *.* /etc/udev/rules.d/
4. Download the image[edit source]
- Create your STM32MP1 Starter Package directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0 mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Starter-Package cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Starter-Package
- Download the STM32MP1-Ecosystem-v5.0.0 Starter Package into the following directory:
$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
tar xvf en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz